Skip to main content
SoHaeng.Lee
Associate III
Jan 29, 2017 4:22 PM UTC
Solved

CubeMX 4.19.0 Problem report.

Posted on January 29, 2017 at 17:22

The attached project is made up of CubeMX 4.18.0.

If you open the project after opening the project at CubeMX 4.19.0 and then creating source again, an error occurs.

    This topic has been closed for replies.
    stm32cube-t
    stm32cube-tBest answer
    ST Employee
    Feb 1, 2017 11:21 AM UTC
    Posted on February 01, 2017 at 12:21

    Hello,

    This is a known issue with MX 4.18.

    Please use the import feature in MX 4.19:

    Start by creating a new project, selecting the STM32F103C8Tx MCU  (as used in your 4.18 project),

    then select the menu File > import to import your 4.18 ioc file.

    You will need to redo the clock tree configuration that could not be automatically imported.

    But, project generation will work fine then.

    2 replies

    ST Technical Moderator
    Jan 29, 2017 8:46 PM UTC
    Posted on January 29, 2017 at 21:46

    Hi

    SoHaeng.Lee

    ‌,

    I will check this issue and come back to you as soon as possible.

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    stm32cube-t
    stm32cube-tBest answer
    ST Employee
    Feb 1, 2017 11:21 AM UTC
    Posted on February 01, 2017 at 12:21

    Hello,

    This is a known issue with MX 4.18.

    Please use the import feature in MX 4.19:

    Start by creating a new project, selecting the STM32F103C8Tx MCU  (as used in your 4.18 project),

    then select the menu File > import to import your 4.18 ioc file.

    You will need to redo the clock tree configuration that could not be automatically imported.

    But, project generation will work fine then.