Skip to main content
Luo.Xinheng
Associate
July 13, 2016
Question

CubeMx 4.15.1 + STM32L476RC + 1.5.1 + FatFS SD

  • July 13, 2016
  • 6 replies
  • 1454 views
Posted on July 13, 2016 at 18:24

hello sir.

my project write SD card error, but it read SD card properly.

when I debug into code, I found 

__HAL_SD_SDMMC_GET_FLAG()

in 

HAL_SD_WriteBlocks()

function

 always get error flag 

SDMMC_FLAG_DCRCFAIL

. and it write nothing to SD card.

I checked my hardware, but it is OK. 

what wrong with my program?

  if(NumberOfBlocks > 1)

  {

    ......

  }

  else

  {

    /* Check for error conditions */

    errorstate = SD_CmdResp1Error(hsd, SD_CMD_READ_SINGLE_BLOCK); 

    

    if (errorstate != SD_OK)

    {

      return errorstate;

    }    

    

    /* In case of single block transfer, no need of stop transfer at all */

   

while(!__HAL_SD_SDMMC_GET_FLAG(hsd, SDMMC_FLAG_RXOVERR | SDMMC_FLAG_DCRCFAIL | SDMMC_FLAG_DTIMEOUT | SDMMC_FLAG_DBCKEND))

    {

      if (__HAL_SD_SDMMC_GET_FLAG(hsd, SDMMC_FLAG_RXFIFOHF))

      {

        /* Read data from SDMMC Rx FIFO */

        for (count = 0; count < 8; count++)

        {

          *(tempbuff + count) = SDMMC_ReadFIFO(hsd->Instance);

        }

        

        tempbuff += 8;

      }

    }   

  }

    This topic has been closed for replies.

    6 replies

    Walid FTITI_O
    Visitor II
    July 14, 2016
    Posted on July 14, 2016 at 14:57

    Hi luo.xinheng,

    It is mentioned in the reference manual that:

    “During block write (CMD24 - 27) one or more blocks of data are transferred from the host to

    the card with a CRC appended to the end of each block by the host. A card supporting block

    write is always able to accept a block of data defined by WRITE_BL_LEN. If the CRC fails,

    the card indicates the failure on the SDIO_D line and the transferred data are discarded and

    not written, and all further transmitted blocks (in multiple block write mode) are ignored.�

    Check if the dummy CRC value is correct ?

    Are you using the ''HW flow control '' ?

    -> Because there is a limitation mentionned in the relevant STM32F40x and STM32F41x Errata sheet:

    ''When enabling the HW flow control by setting bit 14 of the SDIO_CLKCR register to ‘1’, glitches can occur on the SDIOCLK output clock resulting in wrong data to be written into the SD/MMC card or into the SDIO device. As a consequence, a CRC error will be reported to the SD/SDIO MMC host interface (DCRCFAIL bit set to ‘1’ in SDIO_STA register).

    Workaround None. Note: Do not use the HW flow control. Overrun errors (Rx mode) and FIFO underrun (Tx mode) should be managed by the application software

    ''

    -Hannibal-

    Luo.Xinheng
    Associate
    July 14, 2016
    Posted on July 14, 2016 at 16:04

    thanks Hannibal. and I have some problems:

    1. If DCRC error, then no data is writted, it OK;

    2. No matter I use HW flow control or not, the project write SD card error as before.

    3. I don't know how to write or check CRC value, I don't find any CRC function in the stm32CubeMX, Would you tell me where is it?

    4. I have use stm32F411RE, and the program is same approximately, and it work OK. but when I copy it to stm32L476RC, it work wrong.

    5. I only find how to setup  HardwareFlowControl,but how to disable FIFO underrun (Tx mode)?

    /* SDMMC1 init function */

    static void MX_SDMMC1_SD_Init(void)

    {

      hsd1.Instance = SDMMC1;

      hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;

      hsd1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE;

      hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;

      hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;

      hsd1.Init.HardwareFlowControl=SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;

      hsd1.Init.ClockDiv = 0;

    }

    Thanks.

    Walid FTITI_O
    Visitor II
    July 14, 2016
    Posted on July 14, 2016 at 16:57

    Hi luo.xinheng,

    I check the Erratasheet relevant of your device

    http://www.st.com/content/ccc/resource/technical/document/errata_sheet/65/dd/2c/78/59/b0/4c/68/DM00111498.pdf/files/DM00111498.pdf/jcr:content/translations/en.DM00111498.pdf

    and the solution of your problem is there:

    2.7.1 Wrong CCRCFAIL status after a response without CRC is received

    Description

    The CRC is calculated even if the response to a command does not contain any CRC field. As a consequence, after the SDIO command IO_SEND_OP_COND (CMD5) is sent, the CCRCFAIL bit of the SDMMC_STA register is set.

    Workaround

    The CCRCFAIL bit in the SDMMC_STA register shall be ignored by the software. CCRCFAIL must be cleared by setting CCRCFAILC bit of the SDMMC_ICR register after reception of the response to the CMD5 command.

    Apply the workaround and everything will be OK.

    -Hannibal-

    Luo.Xinheng
    Associate
    July 14, 2016
    Posted on July 14, 2016 at 17:22

    Hi,Hannibal.

    I know what wrong with the program.

    In \Drivers\STM32L4xx_HAL_Driver\Inc\stm32l4xx_ll_sdmmc.h , it define 

    #define SDMMC_DATABLOCK_SIZE_1B ((uint32_t)0x00000000)

    #define SDMMC_DATABLOCK_SIZE_2B SDMMC_DCTRL_DBLOCKSIZE_0

    #define SDMMC_DATABLOCK_SIZE_4B SDMMC_DCTRL_DBLOCKSIZE_1

    #define SDMMC_DATABLOCK_SIZE_8B (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_1)

    #define SDMMC_DATABLOCK_SIZE_16B SDMMC_DCTRL_DBLOCKSIZE_2

    #define SDMMC_DATABLOCK_SIZE_32B (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_2)

    #define SDMMC_DATABLOCK_SIZE_64B (SDMMC_DCTRL_DBLOCKSIZE_1|SDMMC_DCTRL_DBLOCKSIZE_2)

    #define SDMMC_DATABLOCK_SIZE_128B

    (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_1|SDMMC_DCTRL_DBLOCKSIZE_2)

    #define SDMMC_DATABLOCK_SIZE_256B             SDMMC_DCTRL_DBLOCKSIZE_3

    #define SDMMC_DATABLOCK_SIZE_512B             (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_3)

    #define SDMMC_DATABLOCK_SIZE_1024B            (SDMMC_DCTRL_DBLOCKSIZE_1|SDMMC_DCTRL_DBLOCKSIZE_3)

    #define SDMMC_DATABLOCK_SIZE_2048B            (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_1|SDMMC_DCTRL_DBLOCKSIZE_3) 

    #define SDMMC_DATABLOCK_SIZE_4096B            (SDMMC_DCTRL_DBLOCKSIZE_2|SDMMC_DCTRL_DBLOCKSIZE_3)

    #define SDMMC_DATABLOCK_SIZE_8192B            (SDMMC_DCTRL_DBLOCKSIZE_0|SDMMC_DCTRL_DBLOCKSIZE_2|SDMMC_DCTRL_DBLOCKSIZE_3)

    #define SDMMC_DATABLOCK_SIZE_16384B           (SDMMC_DCTRL_DBLOCKSIZE_1|SDMMC_DCTRL_DBLOCKSIZE_2|SDMMC_DCTRL_DBLOCKSIZE_3)

    and in \Drivers\CMSIS\Device\ST\STM32L4xx\Include\stm32l476xx.h

    #define SDMMC_DCTRL_DBLOCKSIZE_Pos           (4U)                       

    #define SDMMC_DCTRL_DBLOCKSIZE_0             (0x1U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000010 */

    #define SDMMC_DCTRL_DBLOCKSIZE_1             (0x2U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000020 */

    #define SDMMC_DCTRL_DBLOCKSIZE_2             (0x3U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000040 */

    #define SDMMC_DCTRL_DBLOCKSIZE_3             (0x4U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000080 */

    but we know , it equal define

    #define SDMMC_DCTRL_DBLOCKSIZE_Pos           (4U)                       

    #define SDMMC_DCTRL_DBLOCKSIZE_0           0x10U  /*!< 0x00000010 */

    #define SDMMC_DCTRL_DBLOCKSIZE_1           0x20U  /*!< 0x00000020 */

    #define SDMMC_DCTRL_DBLOCKSIZE_2           0x30U  /*!< 0x00000040 */

    #define SDMMC_DCTRL_DBLOCKSIZE_3           0x40U  /*!< 0x00000080 */

    it is wrong!

    the corrent define is:

    #define SDMMC_DCTRL_DBLOCKSIZE_Pos           (4U)                       

    #define SDMMC_DCTRL_DBLOCKSIZE_0             (0x1U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000010 */

    #define SDMMC_DCTRL_DBLOCKSIZE_1             (0x2U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000020 */

    #define SDMMC_DCTRL_DBLOCKSIZE_2             (0x4U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000040 */

    #define SDMMC_DCTRL_DBLOCKSIZE_3             (0x8U << SDMMC_DCTRL_DBLOCKSIZE_Pos) /*!< 0x00000080 */

    I correct this error, and my program is OK.

    Luo Xinheng

    Walid FTITI_O
    Visitor II
    July 14, 2016
    Posted on July 14, 2016 at 18:35

    Hi luo.xinheng,

    I see now tha you are talking about DCRCFAIL which is not concerned by the Erratasheet note.

    So are you using our hardware or your own ? check the SDIO connection and of there is noise .

    -Hannibal-

    Walid FTITI_O
    Visitor II
    July 15, 2016
    Posted on July 15, 2016 at 11:33

    Hi luo.xinheng,

    Yes, I confirm. It iwill be fixed in the coming firmware library release.

    -Hannibal-