Skip to main content
Associate
Aug 3, 2026 3:20 PM UTC
Solved

CSI_PFCR.DLD bit description contradicts HAL implementation

RM0486 describes CSI_PFCR bit 16 (DLD) as follows:

 
Bit 16 DLD: Data lane direction of lane 0
0: Rx
1: Tx

Per this description, configuring the CSI-2 host to receive from a camera sensor (i.e. lane 0 in RX mode) should require DLD = 0.

However, in the shipped HAL, HAL_DCMIPP_CSI_SetConfig() explicitly sets DLD = 1 (via CSI_PFCR_DLD) when configuring the PHY for CSI-2 RX capture from a camera sensor:

WRITE_REG(csi_instance->PFCR, (0x28U << CSI_PFCR_CCFR_Pos) |
(SNPS_Freqs[pCSI_Config->PHYBitrate].hsfreqrange << CSI_PFCR_HSFR_Pos) | CSI_PFCR_DLD);

The HAL source even contains a comment acknowledging the discrepancy:

/* set basedir_0 to RX DLD 0 RX, 1 TX. Synopsys 1 RX 0 TX  + freq range */

This strongly suggests that the underlying Synopsys D-PHY basedir signal has the opposite polarity (1 = Rx, 0 = Tx) from what's documented for the DLD bit in RM0486, and that the HAL was written/validated against the actual behavior rather than the RM's bit description.

Is this a mistake of myself or a real error in the RM/HAL ?

FBLBest answer
ST Technical Moderator
Aug 6, 2026 8:19 AM UTC

Hi ​@pyven-dr 

DLD bit in CSI_PFCR reflects the external sensor status from the STM32N6 point of view, not the STM32N6 host point of view.

  • DLD = 1 means the external camera sensor is in TX (Transmit) mode.
  • DLD = 0 means the sensor lanes are not actively transmitting HS data.

So, HAL is consistent with the intended meaning; the RM bit description should be clarified. An internal ticket CDM0064937 is submitted to dedicated team.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

FBLBest answer
ST Technical Moderator
Aug 6, 2026 8:19 AM UTC

Hi ​@pyven-dr 

DLD bit in CSI_PFCR reflects the external sensor status from the STM32N6 point of view, not the STM32N6 host point of view.

  • DLD = 1 means the external camera sensor is in TX (Transmit) mode.
  • DLD = 0 means the sensor lanes are not actively transmitting HS data.

So, HAL is consistent with the intended meaning; the RM bit description should be clarified. An internal ticket CDM0064937 is submitted to dedicated team.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
pyven-drAuthor
Associate
Aug 6, 2026 2:06 PM UTC

Thank you for the clarification.