Skip to main content
Moamen Ayman
Associate III
February 25, 2020
Question

Crystal suitable for STM32L4R9AI

  • February 25, 2020
  • 1 reply
  • 658 views

Hello I will use these crystals for STM32L4R9AII6

HSE Crystal 16MHz ±10ppm 8pF 60 Ohms (with external capacitors of 6pf (assuming stray capacitance of 5pf) and ext resistor of 1.6KOhm)

https://www.digikey.com/product-detail/en/jauch-quartz/Q-160-JXS22-8-10-10-WA-LF/1908-1268-1-ND/8108380

RTC CRYSTAL 32768Hz 9pF 20PPM (with external capacitors of 12pf)

https://www.digikey.com/product-detail/en/epson/FC-135-32.7680KA-AC/FC-13532.7680KA-AC-ND/1927426

Is these crystal suitable for this MCU and my values for the external capacitors and resistor correct?

Thanks in Advance!

This topic has been closed for replies.

1 reply

Bowman32
ST Employee
February 25, 2020

Hello,

Both crystals are compatible with STM32L4R9. Also the chosen values of the external capacitors is good.

Please refer to AN2867 (Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs) for more details.

Link to AN2867 : https://www.st.com/content/ccc/resource/technical/document/application_note/c6/eb/5e/11/e3/69/43/eb/CD00221665.pdf/files/CD00221665.pdf/jcr:content/translations/en.CD00221665.pdf

Best regards

Bouraoui