Skip to main content
Visitor II
Mar 20, 2025 2:26 AM UTC
Question

Cross Reference

Pls cross  TI part number TMP75AIDGKR (Temperature Sensor With I2C and SMBus Interface) 

Previously there's a Cross Reference tool in ST website but it's gone. I use it regularly. I hope it can be reinstated. 

6 replies

Peter BENSCH
ST Technical Moderator
Mar 20, 2025 5:56 AM UTC

Welcome @eric_copelan, to the community!

The X-Reference search can still be accessed via the homepage. Depending on the browser, either via a drop-down on the left-hand side of the search field or directly in the search results. Just try it out on st.com!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
Nov 17, 2025 4:42 PM UTC

The cross-reference option is no gone... it was where we could load it in the search bar and it gives us all available crosses.

Peter BENSCH
ST Technical Moderator
Nov 17, 2025 11:05 PM UTC

Welcome @tslater, to the community!

The Xref has not been removed, but is handled differently by different browsers:

Windows Edge

  1. Variant 1
    • Click on the magnifying glass to start the search function.
    • You should then be able to select the angle button to the right of Products.
    • Finally, you should be able to select X-Reference from the list if you only want X-Ref results to be listed:
      • Products
      • Tools & Software
      • Resources
      • Videos
      • Solutions
      • Applications
      • Publications
      • X-Reference
      • All site

  2. Variant 2 (alternative):
    • Click on the magnifying glass.
    • Enter the name of the component you are looking for.
    • If X-References exist for this, a tab X-Reference ({number}) can also be selected in the search results table.

Chrome and, e.g. Brave browser

This is a little more specialised and only allows the above-mentioned alternative function:

  • Enter the name of the component in the search field at the top right and...
  • start the search.
  • In the left-hand column, you will find the bordered Cross References field, at the bottom of which a link show {number} cross references should appear.
  • This link then leads to the same overview.

I'm sorry that it's so hidden, but maybe this will help you.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STLearner
Associate III
Jan 12, 2026 7:25 AM UTC

Hi Peter,

I am facing the same issue and cannot find the icon or the name of cross reference in the search bar. 

Is this function fully removed from ST homepage?

STLearner_0-1768202487389.png

Thanks.

Associate II
Dec 23, 2025 1:38 PM UTC

Hi Peter 

I am also facing same issue, I have attached the image for your reference, previously X reference used to come by clicking on magnify glass option but now, I am not able to click on this option.

Arjun_Bansal_0-1766497051699.png

 

 

Peter BENSCH
ST Technical Moderator
Jan 12, 2026 7:58 AM UTC

As I mentioned above, the behaviour depends on the browser. Since you haven't provided any information other than the screenshot (e.g. operating system, browser, attempted solutions), it's difficult to formulate an answer.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.