Question
creating screens for the STM32L053 Discovery Board
Posted on October 07, 2017 at 07:41
Is there a utility program available that enables one to create custom screens for the STM32L053 Discover Board? I've looked at a couple of demo programs for the E-Paper display and see that the graphics elements are contained within data structures. Is there some kind of a utility program that allows one to create the images visually or import them from a utility program used to create them visually so that they can be added to the various data structures used to build the screens?
#e-paper-display #stm32l053-discovery-board