Skip to main content
thomaspfeffer9
Associate
July 11, 2011
Question

Creating a square wave

  • July 11, 2011
  • 14 replies
  • 6375 views
Posted on July 11, 2011 at 15:01

I'm an absolutly beginner in microcontrollers.

I want to create a simple square wave signal on STM32F103VB with

tim3, ch2, but nothing happens.

Can anybody tell me what I'm doing wrong?

Thanks

Tom

#define DEF_SPEED 140;

#define CCR1_Val  32768;

int main(void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

  TIM_OCInitTypeDef TIM_OCInitStructure;

  // RCC/System clocks configuration

  RCC_Config();

  // Enable Timer3 clock and release reset

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE);

  // map PC7 as TIM3-CH2

  GPIO_InitStructure.GPIO_Pin   = GPIO_Pin_7; //7

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // clock to 50MHz

  GPIO_InitStructure.GPIO_Mode  = GPIO_Mode_AF_PP;  // alternate function pull

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE); // ?!!!!!!!!!!

  // Time base configuration

  TIM_TimeBaseStructure.TIM_Period = 0xFF; // 8 bit resolution

  TIM_TimeBaseStructure.TIM_Prescaler = DEF_SPEED;       

  TIM_TimeBaseStructure.TIM_ClockDivision = 0;    

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 

  TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

  // Output Compare Toggle Mode configuration: Channel2

  TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;          

  TIM_OCInitStructure.TIM_Pulse = CCR1_Val;  

  TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

  TIM_OC2Init(TIM3, &TIM_OCInitStructure);

  TIM_Cmd(TIM3,ENABLE);

 

  while (1) {}

}

    This topic has been closed for replies.

    14 replies

    Tesla DeLorean
    Guru
    June 5, 2014
    Posted on June 05, 2014 at 18:13

    What board and chip are we talking about here? If it's an F100 on a VL-Discovery double check if the chip supports the specific timers

    What other output do you see from your program?

    Do you see output from the non-remapped pins?

    You might need to change the JTAG remapping

       /* Disable the Serial Wire Jtag Debug Port SWJ-DP */

       GPIO_PinRemapConfig(GPIO_Remap_SWJ_Disable, ENABLE);

    or

       /* JTAG-DP Disabled and SW-DP Enabled */

       GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    saudkhanis
    Associate II
    June 5, 2014
    Posted on June 05, 2014 at 18:35

    Sorry i forgot to mention im using STM32F100 Discovery board. I tried using TIM3 full remapping and i was able to get blinking LED (PC9). I thought it might be something to do with CH4 as PC9 is on CH4. With TIM3 partial remapping I was also able to get a pwm on PB1 which again is CH4. If I try to get the output on CH2 (TIM2) or CH1 (TIM3) I dont get the output.

    Tesla DeLorean
    Guru
    June 5, 2014
    Posted on June 05, 2014 at 19:09

    /* Dual PWM Remap Demo PB3/PB4 - STM32 VL-Discovery - sourcer32@gmail.com */
    #include ''stm32F10x.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    // clock for GPIO and AFIO (REMAP)
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
    // clock for TIM2 and TIM3
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2 | RCC_APB1Periph_TIM3, ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    // PB3 TIM2_CH2
    // PB4 TIM3_CH1
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    GPIO_PinRemapConfig(GPIO_FullRemap_TIM2, ENABLE); // Remapped to CH2 PB3
    GPIO_PinRemapConfig(GPIO_PartialRemap_TIM3, ENABLE); // Remapped to CH1 PB4
    /* JTAG-DP Disabled and SW-DP Enabled */
    GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE); // Off PB3/PB4 - REQUIRED
    }
    /**************************************************************************************/
    void TIM2_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz
    TIM_TimeBaseStructure.TIM_Period = 500 - 1; // 1 MHz / 500 = 2 KHz
    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
    // Channel 2 configuration = PB.03 TIM2_CH2
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = (TIM_TimeBaseStructure.TIM_Period + 1) / 2; // 50% Duty
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OC2Init(TIM2, &TIM_OCInitStructure);
    // turning on TIM2 and PWM outputs
    TIM_Cmd(TIM2, ENABLE);
    }
    /**************************************************************************************/
    void TIM3_Configuration(void)
    {
    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
    TIM_OCInitTypeDef TIM_OCInitStructure;
    TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz
    TIM_TimeBaseStructure.TIM_Period = 250 - 1; // 1 MHz / 250 = 2 KHz
    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
    // Channel 1 configuration = PB.04 TIM3_CH1
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = (TIM_TimeBaseStructure.TIM_Period + 1) / 4; // 25% Duty
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OC1Init(TIM3, &TIM_OCInitStructure);
    // turning on TIM3 and PWM outputs
    TIM_Cmd(TIM3, ENABLE);
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    TIM2_Configuration();
    TIM3_Configuration();
    while(1);
    }
    /**************************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {
    }
    }
    #endif

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    saudkhanis
    Associate II
    June 5, 2014
    Posted on June 05, 2014 at 19:19

    Thank you clive1! I will try this now.