Skip to main content
HungKai.Chien
Associate II
October 22, 2020
Question

Could the STM32F103 or STM32F412 support 4GB eMMC nand flash?

  • October 22, 2020
  • 2 replies
  • 1008 views

Our project want to use the 4GB eMMC NAND Flash on STM32F103RC or STM32F412VE.

The eMMC architecture of NAND flash support revision , below. It just require to over the MMC standard 4.41 / 5.1.

Could the STM32F103RC or STM32F412VE support 4GB eMMC NAND flash?

This topic has been closed for replies.

2 replies

TDK
October 22, 2020

Both of them have the hardware to support 4GB eMMC. The HAL support may not be complete. Last I checked the F4 only supported up to 2GB.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
October 22, 2020

Yes, both F1 and F4 should be capable of accessing an eMMC device. You'll be responsible for implementing the driver.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..