Skip to main content
David Littell
Senior II
July 25, 2023
Solved

Cortex M33 fault handlers not being executed

Fault handlers that work on M4 and M7's aren't being executed on an M33.  The Usage Fault I'm creating (via an undefined instruction) appears to be escalated to a Hard Fault.  The Core stops executing instructions before ever reaching a handler.  Is this an artifact of some M33 security BS and if so, how can it be corrected?

Thanks very much for any insight.

This topic has been closed for replies.
David Littell
David LittellBest answer
Senior II
February 16, 2024

In my case the problem was the assembly handlers weren't being marked as Thumb so the Core just bailed on the handler address fetch from the Vector Table.  That little oversight in my .s file took quite a while to ferret out, ugh.

I'm sorry I don't have anything more to offer - all this security sh!t renders the (already daunting) devices *** near unusable.  Good luck.

 

12 replies

Tesla DeLorean
Guru
July 25, 2023

Probably, but "Lockup" is apparently a state..

https://developer.arm.com/documentation/100235/0004/the-cortex-m33-processor/fault-handling/fault-types-reference-table

Perhaps try a divide by zero or unaligned LDRD/STRD.. Might try some of this later, honestly haven't had a reason to explorer, but have L5 and U5 parts.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
David Littell
Senior II
July 25, 2023

Hi Clive, thanks for the reply.  Hope you're well.

The more I read the less I like about this CM33 thing.  It looks like letting any fault escalate to Lockup and having the watchdog pry it out of its hole may be the only viable option.  When somebody asks why the behavior is so different (and so unhelpful) relative to the M4 and M7's I can tell them "next time choose a core that doesn't suck".

Pavel A.
July 25, 2023

Sorry for jumping in. I haven't looked at CM33 good enough, but isn't there a config register similar to CM7, that allows individual handling of these exceptions instead of escalation to HF?

Tesla DeLorean
Guru
July 25, 2023

No worries Pavel, these are the things that need many eyes and insights. On the edge of what I'm doing too.

A quick skim of the docs did suggest you can prioritize, enable/disable and flags some of these things. As I recall there was some flag on other CM models with respect to taking, or not, the divide by zero for example.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Pavel A.
July 26, 2023

Have you looked up how to enable individual exception handlers in CM33? if there's a mechanism similar to CM7, just use it. And leave my reply checked )))

David Littell
Senior II
July 26, 2023

Haha, no check for you!  ;)

Maybe I'm just (more) dense (than usual) but I can't find anything helpful in any document (ARM or ST).

Piranha
Principal III
July 26, 2023
David Littell
Senior II
July 27, 2023

Hi and thanks for the response.  Yes, even with USGFAULTENA set a Usage Fault still escalates to a Hard Fault and ultimately a lockup.

David Littell
Senior II
August 4, 2023

Crickets?

pkulk.1
Associate II
February 16, 2024

Hello David, 

Did you ever get the answer on this question? I am working on similar thing right now.
we have secure project(secure boot, secure services) fault handlers and non secure (threadx, filex, etc) fault handlers.

When I used bad instruction or divide by zero it hits the secure project hard fault handler.

David Littell
David LittellAuthorBest answer
Senior II
February 16, 2024

In my case the problem was the assembly handlers weren't being marked as Thumb so the Core just bailed on the handler address fetch from the Vector Table.  That little oversight in my .s file took quite a while to ferret out, ugh.

I'm sorry I don't have anything more to offer - all this security sh!t renders the (already daunting) devices *** near unusable.  Good luck.