Skip to main content
ksm0100100
Associate
January 5, 2008
Question

cortex and nand flash

Posted on January 05, 2008 at 15:01

cortex and nand flash

    This topic has been closed for replies.

    2 replies

    ksm0100100
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hello all

    i am loking for some advise on the best way to connect a 2GB parallel NAND flash chip to the Cortex-M3

    any help will be greatly appriciated

    thanks

    Kris

    asterix
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hi ksm0100100,

    I have seen on STR7 forums a design connecting 1G and 2Gbytes NAND Flash with STR710 ( ST ARM7 device with External Memory interface) for Mass Storage application and it seems the connection is not complex using only the External Memory Interface Bus and so GPIO for control signal.

    I believe that it would be the same with STM32 coming this Year from ST as

    said by STOne-32 and in ST Datasheets in Future Family enhancement section.

    Another Idea, is to use some of the STM32 GPIOs and using DMA we can make

    the connection easy with minimum CPU loading, Look at

    http://www.st.com/stonline/products/literature/an/13529.pdf

    Section

    ''4.3 GPIO fast data transfer with DMA'' :)

    Magigimix