Question
Cordic Configuration STM32G4
Hello all,
I want to use the Cordic accelerator in a STM32G4 and calculate the atan2 from 2 input arguments. Now two questions arise:
1) Is there a package for CUBE so I can configure it there? Up to now I only see the activation button.
2) If there is no possibility, I configure the peripherals as in the given examples for sine and cosine functions. But which function do I need if I want to calculate the atan2?
Thank you a lot in advance!
Best Regards,
Ben