Question
copy 2 projects to my project, one is PWM, the other one is Examples\ADC
Posted on June 18, 2014 at 21:18
I copy 2 projects into mine, one is PWM, the other one is Examples\ADC\ADC_RegularConversion_DMA. Both of them work perfectly separately
before, but after copied, only one can work.
I
guess it might because some functions occurs 3 times, 1 in the Main(), 1 in PWM, 1 in ADC, like: HAL_Init(); SystemClock_Config(); BSP_LED_Init(LED3);
I delete some, but the program still doesn’t work.
Please help.
Thanks