Skip to main content
alexcarrillo
Associate II
June 23, 2008
Question

Converting temperature

  • June 23, 2008
  • 4 replies
  • 800 views
Posted on June 23, 2008 at 11:25

Converting temperature

    This topic has been closed for replies.

    4 replies

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    temp C = (1.4 - 1715/2^12*3.3)/.0043 + 25

    = 0.01828/.0043 + 25

    = 4.25 + 25

    = 29.25 C +/- 1.5 deg C

    sounds about right

    alexcarrillo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    I'm using the temperature sensor in my SMT32f103. It is configured in the following way:

    Quote:

    // ADC1 configuration

    ADC_DeInit(ADC1);

    ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;

    ADC_InitStructure.ADC_ScanConvMode = ENABLE;

    ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;

    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

    ADC_InitStructure.ADC_NbrOfChannel = 1;

    ADC_Init(ADC1, &ADC_InitStructure);

    // ADC1 regular channels configuration

    // Micro internal temperature sensor

    ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_239Cycles5);

    It looks seems properly (aparently) and I get values from the ADC about 1715. When I convert this value to celsius I obtain 36C that is too much even for the processor temperature.

    I use the formula and the values from the datasheet. Those values are:

    Avg_slope = 4.3 mV/C

    V_25 = 1.4 V

    V_ref = Vdda = 3.3V

    Are those values right? How could I get real values?

    Thanks.

    alexcarrillo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    My value for V25 is 1.43. In the manual the value is between 1.34 and 1.52 but very small variations of this value imply big variations in the result. How could I get a better calibration of this value?

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:37

    Your right it is a very wide range

    V25 Avg_Slope Deg C

    1.34 0.004 14.5715332

    1.43 0.0043 36.22933321

    1.52 0.0046 55.06220279

    looks like the part to part variation is very high, but once calibrated, it's +/- 2deg.

    I guess you need to calibrate each part, power up and quickly take a reading at room temp (before it heats up), it should be 21 deg (or whatever your room temperature is). Compute a bias, store it in FLASH, and add that to any future reading and you should be ok.