Associate II
Apr 18, 2018 3:57 PM UTC
Solved
Converting .bmp to .c can't find the right type
- 2 replies
- 978 views
Posted on April 18, 2018 at 17:57
so i'm using the following function :
BSP_LCD_DrawBitmap();
but i can't find the right conversion from bitmap to .C, i'm in a dead end because i can't use Gui i managed to add all libraries to my project and everything but still even the most simple instructions wont display i would really appreciat your help and thanks
:)
note: the attached file contain a Logo.c file from Cubemx' examples that works fine when i add it, i can't tell what is the type they are using neither the converter