Skip to main content
LMI2
Senior III
July 26, 2015
Question

Connection to F100 Discovery board lost with a Cube project

  • July 26, 2015
  • 7 replies
  • 1174 views
Posted on July 27, 2015 at 01:12

I have a Discovery board with

STM32F100RB MCU

. It looks like this

http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/PF250863?sc=stm32vldiscovery

When I program it with software from it's page

http://www.st.com/web/en/catalog/tools/PF257914

The JTAG/SWD connection is normal but when I program a hex file from Cube the connection is immediately lost.

02:07:19 : [GPIOToggle.hex] opened successfully.

02:07:21 : Memory programmed in 0s and 359ms.

gpiouart1

is a Cube project.

02:07:46 : [gpiouart1 Con1_27_07.hex] opened successfully.

02:07:49 : Memory programmed in 0s and 578ms.

02:07:51 : Disconnected from device.

02:07:51 : Connection to device is lost: check power supply and debug connection.

02:07:51 : If the target is in low power mode, please enable ''Debug in Low Power mode'' option from Target->settings menu.

I can't find any big differences in IDE settings. Only include files are different. So not a Keil problem, I think.

Yes, It is getting late, but what could be the problem.

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    July 27, 2015
    Posted on July 27, 2015 at 13:11

    Does the ST-LINK have current firmware?

    What EXACTLY is the software doing? Classic reasons the debug connection fail are that a) You reprogram the JTAG/SWD pins to other functions, b) You put the part into a low power or standby state.

    Can you regain control with ''Connect Under Reset'', or BOOT0 = HIGH, type approaches?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Nickname5522_O
    Visitor II
    July 27, 2015
    Posted on July 27, 2015 at 13:14

    Hi mich.lei,

    Did you reset the board?

    Could you precise which example of the firmware package you are running?

    -Shahrzed-
    LMI2
    LMI2Author
    Senior III
    July 27, 2015
    Posted on July 27, 2015 at 13:54

    Clive and Shahrzed

    My code does very little, it toggles PC8 and PC9 pins, the leds.of the demo board and sends a test strings along usart (PA10) and PA9. I'll put the code without comments at the end of this message. How is BOOT0 = HIGH command used? I think the ST-link has current firmware, it has ''V1.JS0 STM32 Debugger'' firmware. I have only tried ''stsw-stm32078\an3268\stm32vldiscovery_package\Project\Examples\GPIOToggle\MDK-ARM'' example. I am able to use the card by keeping reset switch down while I click the connect icon, so the board is not lost. This is main.c from the Cube with my code.

    #include ''stm32f1xx_hal.h''
    UART_HandleTypeDef huart1;
    void
    SystemClock_Config(
    void
    );
    static
    void
    MX_GPIO_Init(
    void
    );
    static
    void
    MX_USART1_UART_Init(
    void
    );
    int
    main(
    void
    )
    {
    /* USER CODE BEGIN 1 */
    char
    plii[]=
    ''ghghghghghghg''
    ;
    HAL_Init();
    /* Configure the system clock */
    SystemClock_Config();
    /* Initialize all configured peripherals */
    MX_GPIO_Init();
    MX_USART1_UART_Init();
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_8);
    while
    (1)
    {
    /* USER CODE END WHILE */
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_8);
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_9);
    HAL_UART_Transmit(&huart1,(uint8_t *) plii,
    sizeof
    (plii),3000);
    HAL_Delay(500);
    }
    /* USER CODE END 3 */
    }
    void
    SystemClock_Config(
    void
    )
    {
    RCC_OscInitTypeDef RCC_OscInitStruct;
    RCC_ClkInitTypeDef RCC_ClkInitStruct;
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
    RCC_OscInitStruct.HSIState = RCC_HSI_ON;
    RCC_OscInitStruct.HSICalibrationValue = 16;
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
    HAL_RCC_OscConfig(&RCC_OscInitStruct);
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
    HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
    HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
    }
    /* USART1 init function */
    void
    MX_USART1_UART_Init(
    void
    )
    {
    huart1.Instance = USART1;
    huart1.Init.BaudRate = 115200;
    huart1.Init.WordLength = UART_WORDLENGTH_8B;
    huart1.Init.StopBits = UART_STOPBITS_1;
    huart1.Init.Parity = UART_PARITY_NONE;
    huart1.Init.Mode = UART_MODE_TX_RX;
    huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
    huart1.Init.OverSampling = UART_OVERSAMPLING_16;
    HAL_UART_Init(&huart1);
    }
    void
    MX_GPIO_Init(
    void
    )
    {
    GPIO_InitTypeDef GPIO_InitStruct;
    /* GPIO Ports Clock Enable */
    __GPIOC_CLK_ENABLE();
    __GPIOD_CLK_ENABLE();
    __GPIOA_CLK_ENABLE();
    __GPIOB_CLK_ENABLE();
    GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15|GPIO_PIN_0 
    |GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3|GPIO_PIN_4 
    |GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_10 
    |GPIO_PIN_11|GPIO_PIN_12;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    /*Configure GPIO pins : PD0 PD1 PD2 */
    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
     
    
    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 
    |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7 
    |GPIO_PIN_8|GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13 
    |GPIO_PIN_14|GPIO_PIN_15;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_10 
    |GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14 
    |GPIO_PIN_15|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_5 
    |GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
    /*Configure GPIO pins : PC8 PC9 */
    GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
    GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
    GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    /*Configure peripheral I/O remapping */
    __HAL_AFIO_REMAP_PD01_ENABLE();
    }
    #ifdef USE_FULL_ASSERT
    void
    assert_failed(uint8_t* file, uint32_t line)
    {
    }
    #endif

    Leif
    Tesla DeLorean
    Guru
    July 27, 2015
    Posted on July 27, 2015 at 14:22

    Connect the BOOT[0] pin to VDD?

    Won't this NUKE the debug pins too? WHY are you doing this?

    GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3
    |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7
    |GPIO_PIN_8|GPIO_PIN_11|GPIO_PIN_12|GPIO_PIN_13
    |GPIO_PIN_14|GPIO_PIN_15;
    GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    July 27, 2015
    Posted on July 27, 2015 at 14:25

    PA13 = SWDIO

    PA14 = SWCLK

    This is the debug interface, if you reconfigure/break these pins the debugger won't work, don't do it...
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    LMI2
    LMI2Author
    Senior III
    July 27, 2015
    Posted on July 27, 2015 at 15:21

    That analog pin feature is from the Cube:''Set all free pins as analog (to optimize the power consumption)''. I disabled that setting, but it didn't help.

    Good to to know about the Boot0.

    LMI2
    LMI2Author
    Senior III
    July 28, 2015
    Posted on July 28, 2015 at 12:56

    Any news.

    I have tried what has been suggested. For instance PA13 and PA14 and all the rest are at reset state and so on. It would be nice to know if this is a bug or not.

    /**
    ******************************************************************************
    * File Name : main.c
    * Description : Main program body
    ******************************************************************************
    *
    * COPYRIGHT(c) 2015 STMicroelectronics
    *
    * Redistribution and use in source and binary forms, with or without modification,
    * are permitted provided that the following conditions are met:
    * 1. Redistributions of source code must retain the above copyright notice,
    * this list of conditions and the following disclaimer.
    * 2. Redistributions in binary form must reproduce the above copyright notice,
    * this list of conditions and the following disclaimer in the documentation
    * and/or other materials provided with the distribution.
    * 3. Neither the name of STMicroelectronics nor the names of its contributors
    * may be used to endorse or promote products derived from this software
    * without specific prior written permission.
    *
    * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS ''AS IS''
    * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
    * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
    * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
    * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
    * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
    * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
    * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
    * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    ******************************************************************************
    */
    /* Includes ------------------------------------------------------------------*/
    #include ''stm32f1xx_hal.h''
    /* USER CODE BEGIN Includes */
    /* USER CODE END Includes */
    /* Private variables ---------------------------------------------------------*/
    UART_HandleTypeDef huart1;
    /* USER CODE BEGIN PV */
    /* Private variables ---------------------------------------------------------*/
    /* USER CODE END PV */
    /* Private function prototypes -----------------------------------------------*/
    void
    SystemClock_Config(
    void
    );
    static
    void
    MX_GPIO_Init(
    void
    );
    static
    void
    MX_USART1_UART_Init(
    void
    );
    /* USER CODE BEGIN PFP */
    /* Private function prototypes -----------------------------------------------*/
    /* USER CODE END PFP */
    /* USER CODE BEGIN 0 */
    /* USER CODE END 0 */
    int
    main(
    void
    )
    {
    /* USER CODE BEGIN 1 */
    char
    plii[]=
    ''ghghghghghghg''
    ;
    /* USER CODE END 1 */
    /* MCU Configuration----------------------------------------------------------*/
    /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
    HAL_Init();
    /* Configure the system clock */
    SystemClock_Config();
    /* Initialize all configured peripherals */
    MX_GPIO_Init();
    MX_USART1_UART_Init();
    /* USER CODE BEGIN 2 */
    /* USER CODE END 2 */
    /* Infinite loop */
    /* USER CODE BEGIN WHILE */
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_8);
    while
    (1)
    {
    /* USER CODE END WHILE */
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_8);
    HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_9);
    HAL_UART_Transmit(&huart1,(uint8_t *) plii,
    sizeof
    (plii),3000);
    HAL_Delay(500);
    }
    /* USER CODE END 3 */
    }
    /** System Clock Configuration
    */
    void
    SystemClock_Config(
    void
    )
    {
    RCC_OscInitTypeDef RCC_OscInitStruct;
    RCC_ClkInitTypeDef RCC_ClkInitStruct;
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
    RCC_OscInitStruct.HSIState = RCC_HSI_ON;
    RCC_OscInitStruct.HSICalibrationValue = 16;
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
    HAL_RCC_OscConfig(&RCC_OscInitStruct);
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
    HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
    HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
    }
    /* USART1 init function */
    void
    MX_USART1_UART_Init(
    void
    )
    {
    huart1.Instance = USART1;
    huart1.Init.BaudRate = 115200;
    huart1.Init.WordLength = UART_WORDLENGTH_8B;
    huart1.Init.StopBits = UART_STOPBITS_1;
    huart1.Init.Parity = UART_PARITY_NONE;
    huart1.Init.Mode = UART_MODE_TX_RX;
    huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
    huart1.Init.OverSampling = UART_OVERSAMPLING_16;
    HAL_UART_Init(&huart1);
    }
    /** Configure pins as 
    * Analog 
    * Input 
    * Output
    * EVENT_OUT
    * EXTI
    */
    void
    MX_GPIO_Init(
    void
    )
    {
    GPIO_InitTypeDef GPIO_InitStruct;
    /* GPIO Ports Clock Enable */
    __GPIOC_CLK_ENABLE();
    __GPIOA_CLK_ENABLE();
    /*Configure GPIO pins : PC8 PC9 */
    GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
    GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
    GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    }
    /* USER CODE BEGIN 4 */
    /* USER CODE END 4 */
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void
    assert_failed(uint8_t* file, uint32_t line)
    {
    /* USER CODE BEGIN 6 */
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* USER CODE END 6 */
    }
    #endif
    /**
    * @}
    */
    /**
    * @}
    */
    /************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/