Skip to main content
roman1
Associate II
August 26, 2013
Question

Connecting the JTAG reset signal

  • August 26, 2013
  • 3 replies
  • 4158 views
Posted on August 26, 2013 at 15:47

Hi there

I'm still a bit confused about whether I have to connect the nRESET pin of the 10-pin Cortex Debug Connector to the NRST or the NJTRST pin of the STM32 in case of both JTAG and SWD connection. Could anyone tell?

Regards,

Roman

#jtag
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 26, 2013
Posted on August 26, 2013 at 16:13

NRST/NRESET is the PROCESSOR RESET, this is what you want.

NJTRST is not on this connector. If you need a full JTAG interface, say for boundary scan, you might want to check if you want all the signals on a different connector.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jpeacock2399
Associate III
August 26, 2013
Posted on August 26, 2013 at 21:55

Segger (the J-Link vendor) recommends using JNTRST (the JTAG reset) on pin 10, with an option to connect NRST (procesor reset)  to pin 9.  I use this on an STM32F405 motor controller and it is working with GDB/Segger J-Link/Segger 10 pin adapter combination.

  Jack Peacock
Tesla DeLorean
Guru
August 26, 2013
Posted on August 26, 2013 at 22:39

The use of NRST is however far more common, and viable with J-Link and U-Link. I've reviewed half a dozen schematics and can't see anyone using NJTRST, either on the boards, or converter boards.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..