Skip to main content
Visitor II
August 21, 2024
Solved

Connecting STM32F429I Discovery Board with GT911 capacitive touch display

Hi,

I want to connect the GT911  Capacitive Touch display with the Stm32f429 board,

I got an image on Display using  RGB Data lines through LTDC,

I had a problem with the Gt911 touch Controller Address while I tried to read the gt911 register using I2C, I2C could not find the Gt911 I2C slave Address.

I configured the INT and RST pin according to the GT911 datasheet, but I got the NAK for Both addresses mentioned on the GT911 datasheet.

I have attached Gt911 Documents below, kindly refer.

GT911 touch controller datasheet 

GT911 touch controller programming Guide 

MyCode:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define GT911_INT_PIN GPIO_PIN_15
#define GT911_INT_GPIO_PORT GPIOA

#define GT911_RST_PIN GPIO_PIN_7
#define GT911_RST_GPIO_PORT GPIOA


/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c3;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C3_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void GT911_GPIO_CONFIG(){
	__HAL_RCC_GPIOA_CLK_ENABLE();

	GPIO_InitTypeDef GPIO_InitStruct={0};

	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FAST;

	GPIO_InitStruct.Pin = GT911_INT_PIN | GT911_RST_PIN;
	HAL_GPIO_Init(GT911_INT_GPIO_PORT,&GPIO_InitStruct);

}

void GT911_INT_CONFIG(){

	GPIO_InitTypeDef GPIO_InitStruct = {0};

	GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM;

	GPIO_InitStruct.Pin = GT911_INT_PIN;
	HAL_GPIO_Init(GT911_INT_GPIO_PORT,&GPIO_InitStruct);

}


void GT911_INT_CONTROL(uint8_t state){
	switch(state){
		case 0:
			HAL_GPIO_WritePin(GT911_INT_GPIO_PORT,GT911_INT_PIN,GPIO_PIN_RESET);
			break;
		case 1:
			HAL_GPIO_WritePin(GT911_INT_GPIO_PORT,GT911_INT_PIN,GPIO_PIN_SET);
			break;
		default:
			HAL_GPIO_WritePin(GT911_INT_GPIO_PORT,GT911_INT_PIN,GPIO_PIN_RESET);
			break;

	}
}

void GT911_RST_CONTROL(uint8_t state){
	switch(state){
	case 0:
		HAL_GPIO_WritePin(GT911_RST_GPIO_PORT,GT911_RST_PIN,GPIO_PIN_RESET);
		break;
	case 1:
		HAL_GPIO_WritePin(GT911_RST_GPIO_PORT,GT911_RST_PIN,GPIO_PIN_SET);
		break;
	default:
		HAL_GPIO_WritePin(GT911_RST_GPIO_PORT,GT911_RST_PIN,GPIO_PIN_RESET);
		break;
	}
}
void GT911_Reset_Sequence(void){
	GT911_GPIO_CONFIG();
	MX_I2C3_Init();

	GT911_INT_CONTROL(0);
	GT911_RST_CONTROL(0);

	HAL_Delay(1000);

	GT911_INT_CONTROL(0);

	HAL_Delay(1);

	GT911_RST_CONTROL(1);

	HAL_Delay(6);

	GT911_INT_CONTROL(0);

	HAL_Delay(50);

	GT911_INT_CONFIG();

	HAL_Delay(1000);

}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
// MX_GPIO_Init();
// MX_I2C3_Init();
 /* USER CODE BEGIN 2 */
 GT911_Reset_Sequence();

 uint8_t gesture_id = 0;
//
 HAL_I2C_Mem_Read(&hi2c3, 0xBB, 0x8140, sizeof(uint16_t),gesture_id,sizeof(uint8_t)*1,HAL_MAX_DELAY);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 72;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 3;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2C3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2C3_Init(void)
{

 /* USER CODE BEGIN I2C3_Init 0 */

 /* USER CODE END I2C3_Init 0 */

 /* USER CODE BEGIN I2C3_Init 1 */

 /* USER CODE END I2C3_Init 1 */
 hi2c3.Instance = I2C3;
 hi2c3.Init.ClockSpeed = 100000;
 hi2c3.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c3.Init.OwnAddress1 = 0;
 hi2c3.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c3.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c3.Init.OwnAddress2 = 0;
 hi2c3.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c3.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c3) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Analogue filter
 */
 if (HAL_I2CEx_ConfigAnalogFilter(&hi2c3, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Digital filter
 */
 if (HAL_I2CEx_ConfigDigitalFilter(&hi2c3, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2C3_Init 2 */

 /* USER CODE END I2C3_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, NCS_MEMS_SPI_Pin|CSX_Pin|OTG_FS_PSO_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(ACP_RST_GPIO_Port, ACP_RST_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, RDX_Pin|WRX_DCX_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOG, LD3_Pin|LD4_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : A0_Pin A1_Pin A2_Pin A3_Pin
 A4_Pin A5_Pin SDNRAS_Pin A6_Pin
 A7_Pin A8_Pin A9_Pin */
 GPIO_InitStruct.Pin = A0_Pin|A1_Pin|A2_Pin|A3_Pin
 |A4_Pin|A5_Pin|SDNRAS_Pin|A6_Pin
 |A7_Pin|A8_Pin|A9_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

 /*Configure GPIO pins : SPI5_SCK_Pin SPI5_MISO_Pin SPI5_MOSI_Pin */
 GPIO_InitStruct.Pin = SPI5_SCK_Pin|SPI5_MISO_Pin|SPI5_MOSI_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI5;
 HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

 /*Configure GPIO pin : ENABLE_Pin */
 GPIO_InitStruct.Pin = ENABLE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(ENABLE_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : SDNWE_Pin */
 GPIO_InitStruct.Pin = SDNWE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(SDNWE_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : NCS_MEMS_SPI_Pin CSX_Pin OTG_FS_PSO_Pin */
 GPIO_InitStruct.Pin = NCS_MEMS_SPI_Pin|CSX_Pin|OTG_FS_PSO_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pins : B1_Pin MEMS_INT1_Pin MEMS_INT2_Pin TP_INT1_Pin */
 GPIO_InitStruct.Pin = B1_Pin|MEMS_INT1_Pin|MEMS_INT2_Pin|TP_INT1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : B5_Pin VSYNC_Pin G2_Pin R4_Pin
 R5_Pin */
 GPIO_InitStruct.Pin = B5_Pin|VSYNC_Pin|G2_Pin|R4_Pin
 |R5_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : ACP_RST_Pin */
 GPIO_InitStruct.Pin = ACP_RST_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(ACP_RST_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : OTG_FS_OC_Pin */
 GPIO_InitStruct.Pin = OTG_FS_OC_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(OTG_FS_OC_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : R3_Pin R6_Pin */
 GPIO_InitStruct.Pin = R3_Pin|R6_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF9_LTDC;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : BOOT1_Pin */
 GPIO_InitStruct.Pin = BOOT1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(BOOT1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : A10_Pin A11_Pin BA0_Pin BA1_Pin
 SDCLK_Pin SDNCAS_Pin */
 GPIO_InitStruct.Pin = A10_Pin|A11_Pin|BA0_Pin|BA1_Pin
 |SDCLK_Pin|SDNCAS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 /*Configure GPIO pins : D4_Pin D5_Pin D6_Pin D7_Pin
 D8_Pin D9_Pin D10_Pin D11_Pin
 D12_Pin NBL0_Pin NBL1_Pin */
 GPIO_InitStruct.Pin = D4_Pin|D5_Pin|D6_Pin|D7_Pin
 |D8_Pin|D9_Pin|D10_Pin|D11_Pin
 |D12_Pin|NBL0_Pin|NBL1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);

 /*Configure GPIO pins : G4_Pin G5_Pin B6_Pin B7_Pin */
 GPIO_InitStruct.Pin = G4_Pin|G5_Pin|B6_Pin|B7_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : OTG_HS_ID_Pin OTG_HS_DM_Pin OTG_HS_DP_Pin */
 GPIO_InitStruct.Pin = OTG_HS_ID_Pin|OTG_HS_DM_Pin|OTG_HS_DP_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : VBUS_HS_Pin */
 GPIO_InitStruct.Pin = VBUS_HS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(VBUS_HS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : D13_Pin D14_Pin D15_Pin D0_Pin
 D1_Pin D2_Pin D3_Pin */
 GPIO_InitStruct.Pin = D13_Pin|D14_Pin|D15_Pin|D0_Pin
 |D1_Pin|D2_Pin|D3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pin : TE_Pin */
 GPIO_InitStruct.Pin = TE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(TE_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : RDX_Pin WRX_DCX_Pin */
 GPIO_InitStruct.Pin = RDX_Pin|WRX_DCX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : R7_Pin DOTCLK_Pin B3_Pin */
 GPIO_InitStruct.Pin = R7_Pin|DOTCLK_Pin|B3_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 /*Configure GPIO pins : HSYNC_Pin G6_Pin R2_Pin */
 GPIO_InitStruct.Pin = HSYNC_Pin|G6_Pin|R2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : STLINK_TX_Pin */
 GPIO_InitStruct.Pin = STLINK_TX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
 HAL_GPIO_Init(STLINK_TX_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : G7_Pin B2_Pin */
 GPIO_InitStruct.Pin = G7_Pin|B2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF14_LTDC;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pins : G3_Pin B4_Pin */
 GPIO_InitStruct.Pin = G3_Pin|B4_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF9_LTDC;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 /*Configure GPIO pins : LD3_Pin LD4_Pin */
 GPIO_InitStruct.Pin = LD3_Pin|LD4_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOG, &GPIO_InitStruct);

 /*Configure GPIO pins : SDCKE1_Pin SDNE1_Pin */
 GPIO_InitStruct.Pin = SDCKE1_Pin|SDNE1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF12_FMC;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

if anyone knows the correct steps for initialize or access the GT911 Touch controller, kindly reply.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
August 23, 2024

Hello @Siva1706 ,

See that GT911 driver on github provided by ST for STM32 MCUs: https://github.com/STMicroelectronics/stm32-gt911

See also this thread: https://community.st.com/t5/stm32-mcus-products/does-anybody-have-a-working-code-for-gt911-touch-controller/td-p/630651

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
ST Technical Moderator
August 23, 2024

Hello @Siva1706 and welcome to the Community :),

 

Could you please refer to Discovery kit with STM32F429ZI MCU User manual precisely Table 7. STM32 pin description versus board functions  and check the pin used for display connection.

May Getting started with I2C wiki can help you to start with I2C and to configure pins for Serial Data and Serial Clock.

 

I hope this help you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
August 23, 2024
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.