Skip to main content
Visitor II
March 7, 2025
Question

connect to pixhawk with stm32

when I connect to pixhawk with stm32, I want the channel I want to move according to the data coming from the stick.

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#define IBUS_LENGTH 32
#define ADC_CHANNEL_COUNT 4

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;

UART_HandleTypeDef huart1;

/* USER CODE BEGIN PV */

uint8_t ibus_packet[IBUS_LENGTH];
uint16_t adc_values[ADC_CHANNEL_COUNT];


/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_ADC1_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */


uint16_t adc_to_ibus(uint16_t adc_value)
{
 return (adc_value * 1000 / 4095) + 1000; 
}



void prepare_ibus_packet(uint16_t ch1, uint16_t ch2, uint16_t ch3, uint16_t ch4) {
 ibus_packet[0] = 0x20; 
 ibus_packet[1] = 0x40; 

 uint16_t channels[4] = {
 adc_to_ibus(ch1), 
 1500, 
 adc_to_ibus(ch3), 
 1700 
 };

 for (int i = 0; i < 4; i++) {
 ibus_packet[2 + (i * 2)] = channels[i] & 0xFF; // LSB
 ibus_packet[3 + (i * 2)] = (channels[i] >> & 0xFF; // MSB
 }

 // Kalan kanalları sıfırla
 for (int i = 4; i < 14; i++) {
 ibus_packet[2 + (i * 2)] = 0x00;
 ibus_packet[3 + (i * 2)] = 0x00;
 }

 // Checksum hesapla
 uint16_t checksum = 0xFFFF;
 for (int i = 0; i < 30; i++) {
 checksum -= ibus_packet[i];
 }
 ibus_packet[30] = checksum & 0xFF;
 ibus_packet[31] = (checksum >> & 0xFF;
}


void send_ibus_packet(UART_HandleTypeDef *huart) {
 HAL_UART_Transmit(huart, ibus_packet, IBUS_LENGTH, 100);
}


void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc) {
 if (hadc->Instance == ADC1) {
 prepare_ibus_packet(adc_values[0], adc_values[1], adc_values[2], adc_values[3]);
 send_ibus_packet(&huart1);
 }
}






/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_USART1_UART_Init();
 /* USER CODE BEGIN 2 */

 HAL_ADC_Start_DMA(&hadc1, (uint32_t *)adc_values, ADC_CHANNEL_COUNT);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 HAL_Delay(7);


 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADC1 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ENABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_0;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = 2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = 3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
 */
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = 4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief USART1 Initialization Function
 * None
 * @retval None
 */
static void MX_USART1_UART_Init(void)
{

 /* USER CODE BEGIN USART1_Init 0 */

 /* USER CODE END USART1_Init 0 */

 /* USER CODE BEGIN USART1_Init 1 */

 /* USER CODE END USART1_Init 1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART1_Init 2 */

 /* USER CODE END USART1_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA2_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA2_Stream0_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
March 11, 2025

Hello @juanjuan;

 

Could you please give more details about the issue? Did you receive false data or nothing?

May this Wiki "Getting started with UART - stm32mcu" can help you on how to connect two NUCLEO-L476RG boards using UART.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.