Skip to main content
Visitor II
May 27, 2024
Question

Connect STM32F769I-Discovery to MATLAB/Simulink for PiL-Simulation

Hi guys,

I want to use the STM32F769I-Discovery for a PiL-Simulation in MATLAB/Simulink. As a serial connection I use a USB A to Micro B that is plugged in at the CN15 USB ST-link Port on the microcontroller.. The thing is that when I want to run my model in PiL it doesn't detect the STM32 controller. In the Model Configuration Parameters I checked the COM Port which is in my case COM5. I also installed the ST-Link Debug which is listed in the USB devices section on my device manager.

 

I am thankful for any piece of advice.

This topic has been closed for replies.

1 reply

ST Technical Moderator
September 6, 2024

Hello @Radavidlim11 

It seems you have solved your issue here.

It is recommended to refer to mathworks.com for topics related to STM32 support package. 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL