Skip to main content
Associate III
January 10, 2024
Solved

Confusion about ADC sampling speed and sampled value

Hello.

I am very new in using STM32. I am using STM32H747I-DISCO board. For my project, I only need one ADC in differential mode. Previously, I tried to use DMA with ADC but it never worked, even the "ADC dual mode interleaved" example provided by st didn't work. So, I started to fiddle with "PollForConversion" and interrupt methods. Now, from CubeIDE, i have the following clock setup,

CPU1 - 480 MHz, CPU2 - 240 MHz, APB1 and APB2 timer clocks - 240 MHz, ADC - 21 MHz

Only have channel 1 set to differential mode for ADC1 and Timer 2 in free running (1 MHz) to measure timings.

Here's the timer initialize,

 

static void MX_TIM2_Init(void)
{
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 240;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 4294967295;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
}

Here's the ADC initialize,

static void MX_ADC1_Init(void)
{
 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_8CYCLES_5;
 sConfig.SingleDiff = ADC_DIFFERENTIAL_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 sConfig.OffsetSignedSaturation = DISABLE;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
}

 

I tried both poll and interrupt method and checked the time it takes for reading one sample. From the ADC configuration, it should have 1 Msps sampling rate, that is 1us for each sample. But when checking in action, poll method seems to take about 1 second to read 1 sample (two calls, "PollForConversion" and "GetValue"). Interrupt method seems to take about 400ms. Besides, without any input to ADC pins (0V), the values I get is still very big, roughly 32000 in 16 bit mode and 2000 in 12 bit mode.

 

For my project, I need very fast sampling rate, at least 0.1 Msps, preferably 1 Msps. The processor doesn't have to do anything during sampling. Even the sampled value conversion can be done later. This should be feasible in STM32 microprocessors but I had been unable to do so.

 

Any help or guidance on what I could be doing wrong or what I can improve would be very appreciated. Thank you.

 

This topic has been closed for replies.
TDK
TDKBest answer
January 10, 2024

@Bob S almost certainly has the correct idea here. A bit suspicious that your timeout value is also how long it takes, isn't it?

Note that you need to calibrate the ADC before using it. Again, going off of examples may help. Here is one for ADC polling.

https://github.com/STMicroelectronics/STM32CubeH7/blob/96dd7e5b69d2b10406ac3f358e44b14cececa611/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_RegularConversion_Polling/Src/main.c

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

14 replies

rakib2023Author
Associate III
January 10, 2024

Additionally, since I can't edit the post, if there is any available working sample code for a different board (nucleo, eval or disco) for this particular application, that would also be very appreciated. I don't necessarily have to use H7 series, I can use other boards if it works better or easier.

AScha.3
Super User
January 10, 2024

Hi,

>I don't necessarily have to use H7 series, I can use other boards if it works better or easier.

So why you choose a super-complicated-hi-speed-dual-core-cpu ? to make it more difficult ? :)

What boards you can use ?  (maybe :  nucleo ... F303 ? )

If you feel a post has answered your question, please click on " Best Answer ".
rakib2023Author
Associate III
January 10, 2024

Initially, I had plans to add some computation in the MCU but now I will take anything as long as I get a high-speed ADC working. I am ordering F4 and F7 series nucleo. I will try them separately. I would still prefer to use H7 if I can get the ADC working right since I can offload a good amount of computation to MCU.

TDK
January 10, 2024

> Besides, without any input to ADC pins (0V), the values I get is still very big, roughly 32000 in 16 bit mode and 2000 in 12 bit mode.

Those values are consistent with ~0 V when in differential mode. (32768 and 2048). (Although "no input/floating" and "0V" are not the same.)

Polling for conversion is not practical at 1 Msps. Use HAL_ADC_DMA_Start, put many values into a buffer, and process them periodically on the half- and full-complete interrupt callbacks.

See the ADC_DMA_Transfer examples.

https://github.com/STMicroelectronics/STM32CubeH7/blob/96dd7e5b69d2b10406ac3f358e44b14cececa611/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_DMA_Transfer/Src/main.c

 

As a side note, I want to make sure you're aware that in even in differential mode both inputs must be between 0 V and VREF+.

"If you feel a post has answered your question, please click ""Accept as Solution""."
rakib2023Author
Associate III
January 10, 2024

My initial attempt was to use DMA, of course. But I could not get DMA working at all, even by following official sample codes. From what I gathered, H7 series DMA seems to have some complication. I will try the code you provided. I know that 1 Msps is not realistic without DMA but I will take 100 Ksps if it can be done with poll or interrupt method. But measuring the time shows that either way it's roughly 1~3 sample/s max speed which seems unusually low. Any reason why this might be happening?

TDK
January 10, 2024

Probably your code has a ton of overhead and/or isn't measuring the duration correctly. Show your code.

There's no way an ADC conversion is taking an entire second or even hundreds of ms.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Bob S
Super User
January 10, 2024

Check the return value from HAL_ADC_PollForConversion().  I bet you get HAL_TIMEOUT given that it takes approx 1 sec to return and you pass "1000" as the timeout parameter.  If so, that implies the ADC isn't properly configured/started.

rakib2023Author
Associate III
January 11, 2024

@Bob SThanks a lot. That is something I did not consider.

@TDKI think I've figured out the problem. It was the overrun behavior. CubeMX defaults it to preserved and I didn't change it. Then in debug mode, saw that the first few conversions happen in 2~3 us with return value as 0. Then it starts failing with return value to 3 (HAL_TIMEOUT). Changing overrun behavior to overwritten solved this problem. Now, it shows consistent 2~3 us sampling time. I can work with this. I have yet to try the DMA sample code you provided. Similar code didn't work for my case previously but I will try again.

TDK
TDKBest answer
January 10, 2024

@Bob S almost certainly has the correct idea here. A bit suspicious that your timeout value is also how long it takes, isn't it?

Note that you need to calibrate the ADC before using it. Again, going off of examples may help. Here is one for ADC polling.

https://github.com/STMicroelectronics/STM32CubeH7/blob/96dd7e5b69d2b10406ac3f358e44b14cececa611/Projects/NUCLEO-H743ZI/Examples/ADC/ADC_RegularConversion_Polling/Src/main.c

 

"If you feel a post has answered your question, please click ""Accept as Solution""."