Skip to main content
ABeau.4
Associate
Dec 6, 2021 9:55 PM UTC
Question

Conflict between UART buffer size and Flash erasing on STM32G474

Hi,

I'm having a problem that I simply cannot explain so any help is welcomed.

I'm trying to flash the G4 via UART, to put it simply the app receives a reflash request via UART then it erases the other bank that isnt being used and writes the new double words in it. switchs the bank boot pin then it performs a reset (I used this example as a base :https://github.com/barafael/g4-dual-bank-example)

At first the only code that was sent to tell the mcu that new code was being received was 'R' 'F' but then I decided to also add two bytes to say how many double words will be received.

Increasing the buffer size from 2 to 4 in HAL_UART_Receive_IT() (Line 160) call seems to then block the flash from erasing properly.

/* Private typedef -----------------------------------------------------------*/
typedef enum {
 STANDBY,
 CMDCHECK,	
 PREPARATION,
 FLASH_ERASING,
 FLASH_ERASE_DONE,
 FLASH_WRITE_IN_PROGRESS,
 FLASH_WRITE_DONE,
 UPDATE_DONE,
} updateState_t;
 
// Number of pages for firmware
#define NUM_PAGES 100
 
// Number of bytes for firmware
#define NUM_BYTES NUM_PAGES * FLASH_PAGE_SIZE
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef hlpuart1;
UART_HandleTypeDef huart4;
volatile updateState_t updateState = STANDBY;
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_LPUART1_UART_Init(void);
static void MX_UART4_Init(void);
 
/* Private user code ---------------------------------------------------------*/
uint32_t NUM_DOUBLEWORDS = NUM_BYTES / 8;
 
uint8_t RxBuffer[13]; //Contains the data received by the UART4 via interrupt
 //4 Bytes for the address, 8 for the doubleword and 1 for the checksum
bool newdata = false; //Global flags that tells the programme that new data has been received
struct Line
	{
 uint32_t Address;
	 uint64_t Data;	
	};
	
void HAL_GPIO_EXTI_Callback(uint16_t pin) 
{
 if (pin == GPIO_PIN_13) {
 if (updateState == STANDBY) 
					{
 updateState = PREPARATION;
 }
 }
 
}
 
void HAL_FLASH_EndOfOperationCallback(uint32_t ReturnValue) 
{ 
	if (updateState == FLASH_ERASING && ReturnValue == 0xffffffff) 
	 {
 updateState = FLASH_ERASE_DONE;
 } 
	else if (updateState == FLASH_WRITE_IN_PROGRESS)
	 {
 updateState = FLASH_WRITE_DONE;
 }
}
 
void toggleBankAndReset() 
{
 FLASH_OBProgramInitTypeDef OBInit;
 HAL_FLASH_Unlock();
 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
 HAL_FLASH_OB_Unlock();
 HAL_FLASHEx_OBGetConfig(&OBInit);
 
 OBInit.OptionType = OPTIONBYTE_USER;
 OBInit.USERType = OB_USER_BFB2;
 
 if (((OBInit.USERConfig) & (OB_BFB2_ENABLE)) == OB_BFB2_ENABLE) {
 OBInit.USERConfig = OB_BFB2_DISABLE;
 } else {
 OBInit.USERConfig = OB_BFB2_ENABLE;
 }
 if (HAL_FLASHEx_OBProgram(&OBInit) != HAL_OK) {
 // uint32_t errorCode = HAL_FLASH_GetError();
 while (1) {
 HAL_Delay(1000);
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 }
 }
 if (HAL_FLASH_OB_Launch() != HAL_OK) {
 //uint32_t errorCode = HAL_FLASH_GetError();
 while (1) {
 HAL_Delay(200);
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 }
 }
 HAL_FLASH_OB_Lock();
 HAL_FLASH_Lock();
}
 
uint8_t getActiveBank() 
{
 volatile uint32_t remap = READ_BIT(SYSCFG->MEMRMP, 0x1 << 8);
 return remap == 0 ? 1 : 2;
}
 
int main(void)
{
 /* MCU Configuration--------------------------------------------------------*/
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
	uint8_t UpDone[] = "Update done\r\n";
	uint8_t Bank1[] = "We are in bank 1\r\n";
 uint8_t Bank2[] = "We are in bank 2\r\n";		
 
	uint8_t Ready[] = {'R','D'};
	uint8_t ReqNbDW[] = {'N','D'};
 
	uint8_t BankR[2]; 
	uint8_t LReturn[] = "\r\n";
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_LPUART1_UART_Init();
 MX_UART4_Init();
 HAL_UART_Init(&huart4);
	 uint8_t bank = getActiveBank();
 
 uint32_t last = HAL_GetTick();
 
 uint32_t delay;
 if (bank == 1) 
 {	
 delay = 2000;
 } 
 else 
 {
	delay = 500;
 }
 
 /* Infinite loop */
	bool FromUART = false;
	bool ValidDoubleWord = false;
	bool RQNextDW = false;
	bool EOF = false;
	
	 uint32_t dest = 0x08040000;
	 uint32_t addr;
 uint8_t *src = (uint8_t*) 0x08000000;
	 
	 uint64_t Bothalf;
	 uint64_t Tophalf;
	 uint64_t doubleword;
	 uint64_t CopyDouble;
	
	uint8_t DataAnalyser[sizeof(RxBuffer)];
	
	
	//If I change this size from 2 to 4 the error happens
	HAL_UART_Receive_IT(&huart4,RxBuffer,2); //Get the UART ready to recieve the first data
 
while (1)
 {
		 uint32_t now = HAL_GetTick();
 if (now - last > delay) 
				{
 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 last = now;
 }
 switch (updateState) 
	{case STANDBY:
		 if(newdata) //Set by Rx callback
	 {
		 newdata = false;
		 updateState = CMDCHECK;
		 }			 
 break;
	case CMDCHECK:
	 { 
	 if(RxBuffer[0] == 'R' && RxBuffer[1] == 'F') //Reflash code received
		 {						 
		 updateState = PREPARATION;
	 }
		break;					
 case PREPARATION: //Erase the unused bank
	{
 FLASH_EraseInitTypeDef erase = { 0 };
 erase.TypeErase = FLASH_TYPEERASE_PAGES;
 erase.Banks = bank == 1 ? FLASH_BANK_2 : FLASH_BANK_1;
 erase.NbPages = NUM_PAGES;
 erase.Page = 0;
 
 HAL_FLASH_Unlock();
						__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
 HAL_StatusTypeDef status = HAL_FLASHEx_Erase_IT(&erase);
 if (status != HAL_OK) {
 // TODO error case
 }
 
 updateState = FLASH_ERASING;
 }
 break;
 
 case FLASH_ERASING:
	 delay = 200; //Code gets stuck here
				
 uint32_t ErrCode = HAL_FLASH_GetError();
 
	 break;

This topic has been closed for replies.

1 reply

ABeau.4
ABeau.4Author
Associate
Dec 7, 2021 3:19 PM UTC

After testing around more it seems that the problem is that the RxBuffer array is global. Not sure why that is an issue for the flash