Skip to main content
Emper
Associate II
December 8, 2019
Question

Configuring interrupt pin using CMSIS

Currently I am trying to configure a second interrupt pin using CMSIS.

SYSCFG->EXTICR[1] = (SYSCFG->EXTICR[1] & ~SYSCFG_EXTICR2_EXTI6)|(0b0000 << SYSCFG_EXTICR2_EXTI6_Pos);

 EXTI->FTSR = EXTI_FTSR_TR6;

 EXTI->RTSR = EXTI_RTSR_TR6;

 EXTI->IMR = EXTI_IMR_MR6;

 NVIC_EnableIRQ(EXTI9_5_IRQn);

with void EXTI9_5_IRQHandler(void){} works.

But when I try to add another button for interrupt;

SYSCFG->EXTICR[0] = (SYSCFG->EXTICR[0] & ~SYSCFG_EXTICR1_EXTI3)|(0b0000 << SYSCFG_EXTICR1_EXTI3_Pos);

 EXTI->FTSR = EXTI_FTSR_TR3;

 EXTI->RTSR = EXTI_RTSR_TR3;

 EXTI->IMR = EXTI_IMR_MR3;

 NVIC_EnableIRQ(EXTI3_IRQn);

with void EXTI3_IRQHandler(void){}.

It doesn't do anything...

Why is it that the one above does work and the second one doesn't?

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
December 8, 2019

PA6 and PA3?

Which STM32 model? A "known good" board such as Nucleo/Disco, or something else?

Is PA3 properly connected? Can you see the input level change in respective bit of GPIOA_IDR? Isn't this pin set as Analog in GPIO?

Check in disasm, if the IRQ handler is properly inserted into the vector table.

JW

PS. Change your username to a normal nick.

Emper
EmperAuthor
Associate II
December 8, 2019

Yes, it is PA6 and PA3.

Model is Nucleo F303RE. I guess it really is a software related issue..

GPIOA->MODER = (GPIOA->MODER & ~GPIO_MODER_MODER3)|(0b00 << GPIO_MODER_MODER3_Pos);

 GPIOA->PUPDR = (GPIOA->PUPDR & ~GPIO_PUPDR_PUPDR3)|(0b10 << GPIO_PUPDR_PUPDR3_Pos);

When pushing the button, the interrupt isn't even called

waclawek.jan
Super User
December 8, 2019

Can you see the level changes in IDR?

Is the ISR address inserted in the vector table?

JW

Emper
EmperAuthor
Associate II
December 8, 2019

I think I can test the first one with a seperate program where I toggle a LED.

Not so sure how to test the second question?

waclawek.jan
Super User
December 8, 2019

On Nuclea64, PA3 is connected to STLink's virtual-comm Tx. See the Nucleo's UM1724. Disconnect SB14.

JW

Emper
EmperAuthor
Associate II
December 9, 2019

Didn't know how to disconnect SB14.

I tried changing everything to PC01, still doesn't work.

When I write a program to turn on / off a LED it works fine, so the pin itself is configured right.

The problem lays in the configuration of the interrupt.