Skip to main content
Andrew Chin
Associate II
November 21, 2017
Question

configuring cubemx with F429ZI and ethernet

  • November 21, 2017
  • 1 reply
  • 554 views
Posted on November 21, 2017 at 20:10

I am trying out ethernet with UDP. However, when I generate the files through cube mx, I am unable to get it working like they do in UM1713. 

I tried to compile a project, but it does not like 'ethernetif_input(&gnetif)'. It seems that gnetif is not used anywhere. 

Also, there is no Netif_Config called, so I tried calling it as it is in the manual, but it did not like that either. 

So, I looked for a demo, and I found one with the STM324XG_EVAL. The first thing I noticed was that it did not even include these files in the code generation:

#include 'lwip/opt.h'

#include 'lwip/init.h'

#include 'lwip/netif.h'

#include 'lwip/timeouts.h'

#include 'netif/etharp.h'

#include 'ethernetif.h'

#include 'app_ethernet.h'

#include 'udp_echoserver.h'

Is there something I was supposed to do in CubeMX to include all the needed files?

    This topic has been closed for replies.

    1 reply

    Andrew Chin
    Associate II
    November 21, 2017
    Posted on November 21, 2017 at 20:18

    Also, LWIP middle ware and the Ethernet driver are enabled.