Skip to main content
PCTM
Associate
December 12, 2022
Question

Configure SPI or I2C for continuous clock

  • December 12, 2022
  • 6 replies
  • 1648 views

In our STM32L5 based design we are using HSI16 to drive some clocks (SPI1). one way to route HSI16 clock is through MCO. is there any other way we can route this clock.

1. Can we configure I2C or SPI1 to route its clock on some GPIOs ?

2.Continuous write ,dummy write, on to I2C or SPI is good enough to generate clock ?

This topic has been closed for replies.

6 replies

Pavel A.
December 13, 2022

Use a timer for pulse output?

Piranha
Principal III
December 13, 2022

Beyond MCO the next simplest is a timer output channel.

S.Ma
Principal
December 13, 2022

Agreed that timer pwm is the logical next choice. However to answer the original question, yes, you can use spi master transmit mode to generate a pseudo clock using DMA cyclic TX a single data byte 0x55....

PCTM
PCTMAuthor
Associate
December 14, 2022

Thank you for inputs.

Sorry i missed one imp ask, we are trying for clean clock or its mimic. Any change in phase of clock or delay/stretch in clock will affect our test.

we tried timer, but timer roll out will add 'glitch' in our measurement.

Tried I2C but AUTOEND will add phase shift in clock.

SPI with DMA one which i am trying, hope this will give clean clock.

our effort is in getting clock as good as it is out-of-osc kind. Since MCO is not-reachable in our design we are looking for alternate solution.

Thank you again for taking time out, to respond.

Sem A.
Visitor II
December 22, 2022

This forum thread was marked by the moderator as needing a little more investigation, so a support case was created in your name and will be handled off-line. Should anyone have any related questions, please feel free to open a Support case directly at your myST portal: http://community.st.com/s/onlinesupport

Piranha
Principal III
December 23, 2022

> timer roll out will add 'glitch'

Timer can generate perfect pulses without any glitches. You just have to program it properly.