Skip to main content
Associate II
September 30, 2024
Solved

Configuration of VDD50USB and VDD33USB Pins When USB Functionality is Not Used

Hello ST Community,

I am seeking guidance on how to properly configure the VDD50USB and VDD33USB pins on our STM32 device when we are not utilizing the USB functionality. The explanations provided in the datasheet and application notes are somewhat ambiguous and do not explicitly address the scenario where the USB functionality is not utilized.

Could anyone provide detailed instructions or best practices for configuring these pins in such cases?

 

Thank you!

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
October 14, 2024

Hi @ManjuMulimani 

 

Check this FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

I hope this would be helpful.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

TDK
September 30, 2024

"connect VDD33USB to GND (saves some supply current), leave VDD50USB unconnected and make sure that the VDD33USB supply level detector is disabled."

Solved: STM32H745 - USB power pins - connect to VDD or Ope... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."
FBLBest answer
ST Technical Moderator
October 14, 2024

Hi @ManjuMulimani 

 

Check this FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

I hope this would be helpful.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL