Skip to main content
Senior II
Nov 19, 2026 8:31 PM UTC
Question

Concern over stock levels - STM32L433RCT6P

I have spent the last 18 months working on a device that I hope will soon go into production which uses the STM32L433RCT6P.

I am about to get a pre-production board fabricated and assembled, but there is a hold up because STM32L433RCT6P is out of stock.

Digikey are due to receive 810 in stock next month, but then the next re-stock will only be 150 and will not be until the end of next year  !

This is very concerning if my device soon goes into production, its already causing a delay to my pre-production board.

  1. The website shows the part is active, so presumably its not about to go obsolete ?
  2. Are stock levels an issue with all STM32 devices ?
  3. Do I need to consider changing to a different part ?
  4. If I have to change to a different part, is there a compatible replacement (preferably with no or minimal changes to hardware and firmware)