Skip to main content
Marco Israel
Associate II
Dec 30, 2017 2:30 PM UTC
Solved

Compiler erros in stm32l4xx_ll_usart.h and stm32l4xx_ll_rcc.h

Posted on December 30, 2017 at 15:30

Hello together,

I try to make my first, baby steps with cortex controller.

Currently I try to set up an USART and using the free edition of uVision 5. When I try to compile my code I get about 2*30erros out of  stm32l4xx_ll_usart.h (which I had copied in my project folder.) which are always the both below:

_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *

SARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #90: function returning function is not allowed

_STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *

SARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(649): error: #141-D: unnamed prototyped parameters not allowed when body is present

__STATIC_INLINE void LL_USART_EnableDirectionTx(USART_TypeDef *USARTx)

_SRC\../_HDR/../_HDR/stm32l4xx_ll_usart.h(660): error: #79: expected a type specifier

Does someone has any ideas? I also try to compile a project out of the example folders. This works fine without any erros (exapt that I cant recieve any information via usart in my terminal. Maybe the lib doesent work correct? But that is an other problem for a new thread ...). So I try to check and copy the project setting. But without success, unfortunately. Still about 60 compiler erros...

    This topic has been closed for replies.
    Marco Israel
    Marco IsraelBest answer
    Associate II
    Jan 4, 2018 12:24 PM UTC
    Posted on January 04, 2018 at 13:24

    I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..  

    1 reply

    Marco Israel
    Marco IsraelAuthorBest answer
    Associate II
    Jan 4, 2018 12:24 PM UTC
    Posted on January 04, 2018 at 13:24

    I don't know, what I have done (maybe cleaning the project, delete the files and add it new to the project). But the errors are gone now... Don't know ..