Skip to main content
teslashock
Associate II
January 18, 2012
Question

Compilation problems for stm32

  • January 18, 2012
  • 1 reply
  • 678 views
Posted on January 18, 2012 at 04:38

I have set up my toolchain under WinXP like that:

1. downloaded codesourcery LITE g++, installed it 2. downloaded Eclipse with C/C++ support 3. downloaded GNU ARM PLUGIN for Eclipse, and installed it from Eclipse directly after that i could see the code sourcery toolchain in my settings file, i.e. all set up fine. now i do the following: 1. i create the empty project with some very simple main.c which adds numbers. 2. i download the version 3.5.0 peripheral access library from st. 3. i copy the following files from that library to my project folder: stm32f10x.h system_stm32f10x.h core_cm3.h and then i of course include them in project, as well as include ''stm32f10x.h'' file from the main.c file. then i copy the following startup file from that peripheral library: startup_stm32f10x_hd.s i also include the basic linker script with memory mapping for HD devices. the linker script looks like this:

MEMORY
{
sram (W!RX) : ORIGIN = 0x20000000, LENGTH = 64k
flash (RX) : ORIGIN = 0x08000000, LENGTH = 512k
}
SECTIONS
{ 
.text :
{
. = ALIGN(4);
_text = .;
PROVIDE(stext = .);
KEEP(*(.isr_vector))
KEEP(*(.init))
*(.text .text.*) 
*(.rodata .rodata.*) 
*(.gnu.linkonce.t.*)
*(.glue_7)
*(.glue_7t)
*(.gcc_except_table)
*(.gnu.linkonce.r.*)
. = ALIGN(4);
_etext = .;
_sidata = _etext;
PROVIDE(etext = .); 
_fini = . ;
*(.fini)
} >flash
.data : AT (_etext)
{
. = ALIGN(4);
_sdata = .;
*(.ramfunc .ramfunc.* .fastrun .fastrun.*)
*(.data .data.*)
*(.gnu.linkonce.d.*)
. = ALIGN(4);
_edata = .;
} >sram
.ARM.extab :
{
*(.ARM.extab*)
} >sram
__exidx_start = .;
.ARM.exidx :
{
*(.ARM.exidx*)
} >sram
__exidx_end = .;
.bss (NOLOAD) : {
. = ALIGN(4);
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .;
*(.bss .bss.*)
*(.gnu.linkonce.b.*)
*(COMMON)
. = ALIGN(4); 
_ebss = .;
} >sram
end = .;
PROVIDE( _estack = 0x20010000 );
}

but during compile it gives me errors like: undefined reference to _fstat etc... in the project properties i did browse and pointed it to the .ld linker script shown above... so what could be a problem?
    This topic has been closed for replies.

    1 reply

    teslashock
    Associate II
    January 18, 2012
    Posted on January 18, 2012 at 06:01

    ok its because i had printf function forgotten in main code... removed it, it worked.