Skip to main content
nagendrapilladi
Associate II
March 13, 2008
Question

compilation issue

  • March 13, 2008
  • 3 replies
  • 736 views
Posted on March 13, 2008 at 09:12

compilation issue

    This topic has been closed for replies.

    3 replies

    lanchon
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    where did you get the linker scripts from?

    nagendrapilladi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi,

    i use codesourcery g++ lite. i used ld - T generic.hosted.ld stm32.ld

    i got main.bin file size more in MBs.I want use sprintf ,printf function.

    what is the procedure to do ld?

    following files size:

    Volume in drive D is Data

    Volume Serial Number is 681B-B60B

    Directory of D:\nagendra\Example7

    03/13/2008 10:38 AM .

    03/13/2008 10:38 AM ..

    03/13/2008 10:12 AM lib

    03/13/2008 10:36 AM 402,653,192 main.bin

    03/13/2008 10:15 AM 8,885 main.c

    03/13/2008 10:36 AM 152,026 main.elf

    03/13/2008 10:36 AM 103,545 main.elf.map

    10/08/2007 12:50 AM 2,580 main.h

    03/13/2008 10:36 AM 6,128 main.o

    03/13/2008 10:36 AM 1,915 makefile

    03/13/2008 10:37 AM 104 nagen

    10/08/2007 12:50 AM 2,759 readme.txt

    02/01/2008 12:18 AM 973 stm32.ld

    10/08/2007 12:50 AM 5,570 stm32f10x_conf.h

    10/08/2007 12:50 AM 22,695 stm32f10x_it.c

    10/08/2007 12:50 AM 3,267 stm32f10x_it.h

    03/13/2008 10:36 AM 13,128 stm32f10x_it.o

    03/13/2008 10:38 AM 0 test.txt

    15 File(s) 402,976,767 bytes

    3 Dir(s) 19,790,196,736 bytes free

    is there any solution to resolve size ?

    regards

    nagendra

    nagendrapilladi
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi,

    I use stm32.ld in stm32fwlib folder.

    what to do resolve the size and how to use c printf functions using that examples ? is there any procedure to add more linking and compile options?

    can any one help me ?