Skip to main content
Associate
November 6, 2023
Question

Compatible SDIO voltage translator for STM32F413

  • November 6, 2023
  • 3 replies
  • 1578 views

Hi,

We are designing STM32F413ZHJ6 at 1.8V and are looking for a suitable level translator to 3.3V for the on-board microSD connector. I'm considering NXS0506UP or NVT4858. Just wondering if these parts would be compatible with the STM32? Any suggestion?

Thanks,

Thai

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
November 6, 2023

Perhaps, but I don't recall the F4 having a direction pin, or a clock feedback path. Some of the H7 have this to facilitate a buffer, and lower voltages in Ultra / DDR modes, etc.

Suspect you'd need to prototype and test.

There are eMMC that will work at 1.8V as I recall

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ThaiAuthor
Associate
November 7, 2023

Hi Tesla,

Thanks. The STM32F4 only supports SDIO v2.00 so it will only be running in non-UHS modes. The translators I shared are auto-directional so direction pin should not be required.

I don't entirely understand the purpose of clock feedback (provided by most SDIO voltage translators) and when  would it be required. Could you share some thoughts? 

Tesla DeLorean
Guru
November 7, 2023

The feedback clock allows the peripheral to handle the delay / skewing of the signals across the shifter in the return path.

I'd want to see this work before building hundreds of boards.

Look at H7 rather than F4

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..