Skip to main content
elmzaiti youssef
Associate III
July 12, 2017
Question

compatibility between LL library of stm32f4 and stm32f7

  • July 12, 2017
  • 3 replies
  • 910 views
Posted on July 12, 2017 at 13:35

the LL library of the stm32f4xx and stm32f7xx , is the same ?

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    July 12, 2017
    Posted on July 12, 2017 at 14:14

    Hello

    youssef.elmzaiti

    ,

    To see more about Low layer drivers on STM32F7 and STM32F4, refer to the user manual:

    With Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Tilen MAJERLE
    ST Employee
    July 14, 2017
    Posted on July 14, 2017 at 10:24

    Hello

    youssef.elmzaiti

    ‌,

    LL libraries are designed for very low-level tasks and there is general compatibility between them, but this is not the case for all peripherals. There can be incompatibility and some functions which exists in F7, are not available on F4, depends on device features, and vice-versa of course.

    elmzaiti youssef
    Associate III
    July 19, 2017
    Posted on July 19, 2017 at 15:49

     ,

     ,

    2017-07-14 10:24 GMT+02:00 Tilen MAJERLE <,st-microelectronics@jiveon.com>,:

    STMicroelectronics Community

    <,https://community.st.com/?et=notification.mention>,

    You have been mentioned

    by Tilen MAJERLE

    <,

    Re: compatibility between LL library of stm32f4 and stm32f7 in

    STMicroelectronics Community* - View Tilen MAJERLE's reference to you

    <,https://community.st.com/0D70X000006Sp8aSAC