Skip to main content
Alex Golubev
Associate III
May 20, 2021
Question

Communication error via virtual com port when reconnecting

  • May 20, 2021
  • 0 replies
  • 493 views

When the USB CDC vertical com port is disconnected at the time of data transfer, an error cannot be generated (Code 29). Full name of the error "The device is disabled because the control firmware of the device has not received the requested resources from the system. (Code 29)".

At the time of reconnection, the variable (((USBD_CDC_HandleTypeDef *) hUsbDeviceFS.pClassData) -> TxState is not equal to zero. hUsbDeviceFS parameter.dev_state = USBD_STATE_CONFIGURED

I use the stm32h743 microcontroller, the stm32cubeide programming environment, _HAL.

This topic has been closed for replies.