Skip to main content
FLast.5
Associate II
Dec 16, 2019 1:38 AM UTC
Solved

Communicating 10 STM32F429x parallelly with PC program.

I have to connect 10 devices based on STM32F429x MCU to PC and run them in parallel and send log data from all those STM32F429x devices to PC.

Previously when using 1-2 ARM devices with PC I had been using serial port with RS3232 and USB-serial converter to transfer data from my device to PC. My PC program is written in C# using its serial port interface.

The data size transferred from device to PC is 1~2 Kb per device and control signals to individual devices (few bytes). All of them need to run parallelly and will probably send data at almost same time. Timing for log data transmission depends on completion of tasks in each ARM devices but there is no big difference on completion of tasks (probably ~300 ms difference maximum). And the result is to be displayed in PC in real time.

For 10 devices, I don't know if RS3232 would be problem. I do not want to go with USB expansion hub because the ports keep changing whenever PC reboots. Can I use RS-3232 and USB-serial converter with Serial expansion card or Ethernet-Serial converter connected to router to PC ? (Ethernet-Serial converter to avoid IP related complexities.)

If I go with Ethernet method what should be the communication mechanism in c# ?

I want to know which one would be better solution.

Thank you.

This topic has been closed for replies.

10 replies

berendi
Principal
Dec 16, 2019 3:36 AM UTC

What best suits your situation is depending on your requirements. How much data, what latency?

FLast.5
FLast.5Author
Associate II
Dec 17, 2019 6:31 AM UTC

Data is 1-2 Kb. Time delay among each transmitting devices 300 ms at maximum.

Ozone
Principal
Dec 17, 2019 8:31 AM UTC

That should be manageable.

Assuming Windows as host OS, I still suggest do some proper planning beforehand.

Most USB-serial adapters state their driver chip, including internal buffer (FIFO) capacity. I would go for one documenting such features.

Considering your baudrate, you can configure your host USB driver (poll rate and buffer size) according to your requirements.

Ozone
Principal
Dec 16, 2019 7:20 AM UTC

You can tinker with the packet size and latency (poll rate) of the USB driver on PC side, to avoid data loss.

If you do not run each of the nodes at full bandwidth capacity, a decent PC should be capable of handling it - most of the time.

But Windows (and Linux or MacOS) is no real-time OS, it will faint in high-load situations.

If can't have data loss/overrun, use handshake and a safe protocol.

FLast.5
FLast.5Author
Associate II
Feb 20, 2020 1:54 AM UTC

So far no problem with data loss and praying such would not occur. Set my baud-rate at 115200.

Piranha
Principal III
Dec 17, 2019 10:03 AM UTC

You can do it using RAW Ethernet without IP stack. Here is what you get "for free" with Ethernet hardware:

  • Collision avoidance.
  • Data messages instead of stream.
  • Scatter/gather DMA.
  • CRC checking.
  • Robust physical connection.
  • Vast scalability with switches, which also do additional frame buffering.
  • No additional hardware needed on PC side.

Also note that on the MCU side sending/receiving RAW Ethernet frames is far more easier than dealing with USB stack. It's even easier than managing USART properly!

On a PC side: https://stackoverflow.com/questions/3964013/how-send-raw-ethernet-packet-with-c

Jack Peacock_2
Associate II
Dec 17, 2019 2:33 PM UTC

Another alternative is to replace the RS-232 with half-duplex RS-485, assuming your 10 devices are relatively close together (meter or more separation, 1km end to end). On the PC side use a USB to RS-485 adapter, which appears as a COM port on the PC. Use the COM port API in C# to communicate.

With RS-485 all devices share a common bus. The STM32s listen for an address command from the PC, and then the selected device responds with data back to the PC. There is the added complication of half-duplex with line turnaournd but this isn't difficult to implement. If you want to use a standard protocol for this take a look at Modbus.

RS-485 is a very common industrial interface used to replace RS-232 when devices are networked, or if noise immunity is an issue. RS-485 can operate at higher speeds over a longer distance with greater reliability compared to RS-232.

BTW if you see a USB device constantly changing ports when connected to a PC it's because the USB device is not reporting a serial number to uniquely identify itself. The PC has no way of knowing you are using the same adapter more than once. A well made USB device will always report a serial number, allowing the OS to assign a fixed COM port for serial.

Jack Peacock

Pavel A.
Pavel A.Best answer
Dec 18, 2019 1:51 AM UTC
FLast.5
FLast.5Author
Associate II
Feb 20, 2020 1:49 AM UTC

This is working great for me. Thanks.