Skip to main content
Mvega
Associate
January 22, 2019
Question

Communicate with I2C a STM32 and a Raspberry

I want to connect a Raspberry Pi and a STM32F446 via I2C. I want the STM to be the slave. The code on the Raspberry is ok because I am already connected to other devices but when i search for the adress of the STM it doesn't appear. I'm sure the problem is with the init bu can't find it. I attach the code of the init.

Thanks in advance.

void I2C_Init(void){

GPIO_InitTypeDef GPIO_InitStruct;

I2C_InitTypeDef I2C_InitStruct;

RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C3, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_Init(GPIOA, &GPIO_InitStruct);

GPIO_InitStruct.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;

GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_InitStruct.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_Init(GPIOC, &GPIO_InitStruct);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_I2C3); //SCL

GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_I2C3); //SDA

I2C_InitStruct.I2C_Mode = I2C_Mode_SMBusDevice;

I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2;

I2C_InitStruct.I2C_OwnAddress1 = 0x10;

I2C_InitStruct.I2C_Ack = I2C_Ack_Enable;

I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

I2C_InitStruct.I2C_ClockSpeed = 100000;

I2C_DeInit(I2C3);

I2C_Init(I2C3, &I2C_InitStruct);

I2C_Cmd(I2C3, ENABLE);

}

This topic has been closed for replies.

4 replies

S.Ma
Principal
January 23, 2019

It might be easier to implement SPI link between both devices, and bit rate should easily be 12 mbps or higher.

Mvega
MvegaAuthor
Associate
January 23, 2019

I know but for my case i can only use I2C...

Mvega
MvegaAuthor
Associate
January 28, 2019

solved

AlexSh
Visitor II
July 29, 2019

I'm also struggling with connecting STM32 to RPi as a slave. Could you please share you solution?