Question
Combining Input Capture, One-Pulse Mode, and Reset Mode
Posted on October 07, 2014 at 16:28
I am using an STM32F407xx.
My setup is that I have TIMa triggering TIMb. Here is a description of the behavior that I want:TIMa:Don't care. This part looks to be working in my application.TIMb:- When we get a Trig:
- Capture the current value of TIMb->CNT into CCR1
- Reset TIMb->CNT to 0.
- TIMb should start counting again from 0.
- If TIMb->CNT == TIMb->ARR,
- Stop Counting
- Fire an interrupt
- When we get another Trig:
- Capture TIMb->ARR into TIMb->CCR1
- Reset TIMb->CNT to 0
- TIMb should start counting again from 0.
How can I accomplish this?
Here is what I have found so far:- Setting the TIMb trig source will allow it to react to TIMa
- Setting up CC1 as an input capture will allow the trigger to capture the current timer value
- Setting the TIMb in Reset slave mode will set TIMb->CNT = 0 every trigger
- I have been unable to get the stopping at TIMb->CNT == TIMb->ARR part to work
- My initial plan was to use the timer one-pulse mode
- I wanted this to do the timer stopping
- This does not appear to let the CC1 channel function properly
- I experimented with the URS and UDIS bits to no avail.
- My initial plan was to use the timer one-pulse mode
Any pointers here?
#reset #one-pulse #timers #stm32f4