Skip to main content
stthormj9
Associate II
August 2, 2016
Question

Com port on Nucleo F030 board?

  • August 2, 2016
  • 9 replies
  • 1770 views
Posted on August 02, 2016 at 03:06

I  used the mbed compiler to make and download the Nucleo_printf program, but I'm not getting any serial output.  I'm using Tera Term on Com23 @ 9600-8-n-1, no flow control.

Is there a step I'm missing?

What baud rates does the VCP support?  Do you have to enable it before using it?

#nucleo
    This topic has been closed for replies.

    9 replies

    Tesla DeLorean
    Guru
    August 2, 2016
    Posted on August 02, 2016 at 03:28

    I don't use mbed. The VCP should work at 9600 8N1 or 115200 8N1 without issues. On other Nucleo boards this is USART2 with PA2/PA3, you'd need to double check the board for the F030

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 2, 2016
    Posted on August 02, 2016 at 04:28

    Here is how I've used them in C

    /* STM32 USART2 PA.2 Tx, PA.3 Rx STM32F030R8 NUCLEO sourcer32@gmail.com */
    #include ''stm32f0xx.h''
    /**************************************************************************************/
    void RCC_Configuration(void)
    {
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE);
    }
    /**************************************************************************************/
    void GPIO_Configuration(void)
    {
    GPIO_InitTypeDef GPIO_InitStructure;
    // PA.2 USART2_TX, PA.3 USART2_RX
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1);
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1);
    /* Configure USART2 pins: Rx and Tx ----------------------------*/
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    }
    /**************************************************************************************/
    void USART2_Configuration(void)
    {
    USART_InitTypeDef USART_InitStructure;
    USART_InitStructure.USART_BaudRate = 9600;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    USART_Init(USART2, &USART_InitStructure);
    USART_Cmd(USART2,ENABLE);
    }
    /**************************************************************************************/
    void OutString(char *s)
    {
    while(*s)
    {
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART2, *s++); // Send Char
    }
    }
    /**************************************************************************************/
    int main(void)
    {
    RCC_Configuration();
    GPIO_Configuration();
    USART2_Configuration();
    OutString(''Welcome to Nucleo F030R8
    
    '');
    while(1)
    {
    uint16_t Data;
    while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Char
    Data = USART_ReceiveData(USART2); // Collect Char
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
    USART_SendData(USART2, Data); // Echo Char
    }
    }
    /**************************************************************************************/
    #ifdef USE_FULL_ASSERT
    /**
    * @brief Reports the name of the source file and the source line number
    * where the assert_param error has occurred.
    * @param file: pointer to the source file name
    * @param line: assert_param error line source number
    * @retval None
    */
    void assert_failed(uint8_t* file, uint32_t line)
    {
    /* User can add his own implementation to report the file name and line number,
    ex: printf(''Wrong parameters value: file %s on line %d
    
    '', file, line) */
    /* Infinite loop */
    while (1)
    {}
    }
    #endif
    /**************************************************************************************/

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stthormj9
    stthormj9Author
    Associate II
    August 2, 2016
    Posted on August 02, 2016 at 20:30

    Ok weird.  My reply didn't show up so I'm going to post it again...

    What kit does this work with?  Mine (Keil uvision 5, STM32Cube HAL v 1.4.0) is complaining about many unresolved symbols.

    Tesla DeLorean
    Guru
    August 2, 2016
    Posted on August 02, 2016 at 21:08

    I use the Standard Peripheral Library (SPL), bottom of the page if you ignore all the Cube stuff.

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries/stsw-stm32048.html

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stthormj9
    stthormj9Author
    Associate II
    August 2, 2016
    Posted on August 02, 2016 at 21:35

    Ok, that goes a long way.  How do you configure the SPL for the processor (I'm getting messages about USART3 and PORTE -- which are not on this micro)?

    Thank you very very much!

    Tesla DeLorean
    Guru
    August 2, 2016
    Posted on August 02, 2016 at 22:40

    Set compiler defines

    USE_STDPERIPH_DRIVER,STM32F0XX

    or

    USE_STDPERIPH_DRIVER,STM32F030,USE_DEFAULT_TIMEOUT_CALLBACK

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stthormj9
    stthormj9Author
    Associate II
    August 3, 2016
    Posted on August 03, 2016 at 14:23

    Ok, got it to compile -- I first got the usart_printf example in StdPeriph to compile (but that didn't work), then I replaced the main.c with your example.  Still compiles.  But I don't see any output on the serial port nor if I hook a oscilloscope to PA2... and I can't figure out why -- the code seems straightforward.

    I've tried with 2 F030R8 nucleo boards -- was there a bad batch of STM32F030R8's (or nucleo -- but if that's the case I should still see it in the oscilloscope)?

    stthormj9
    stthormj9Author
    Associate II
    August 3, 2016
    Posted on August 03, 2016 at 20:04

    A-ha!  After I made the bouncy program, I still couldn't see anything.  Looking through the schematics, you have to make SB62 & SB63 so you can see it on the expansion connectors -- did that, and now I see serial traffic on the oscope.

    The VCP doesn't seem to work, but I'll make a new thread for that now that I have serial working.  Many thanks for helping me with this, @clive1!

    Tesla DeLorean
    Guru
    August 3, 2016
    Posted on August 03, 2016 at 21:10

    I used it on a stock Nucelo F030 board last night, no modifications.

    You should be able to see the VCP pins at CN3 RX/TX by the SWD header. Using ClearTerminal at 9600 8N1. Will double check the VCP driver version when I get back.

    Have it send 'U' in a loop, scope that and double check baud rate.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..