Skip to main content
bl_it
Associate III
March 26, 2013
Question

Code Red / Red Probe with the 32F4 DISCOVERY board

  • March 26, 2013
  • 12 replies
  • 1732 views
Posted on March 26, 2013 at 12:43

Hi Folks 

I just thought that I would say that using the Code Red tools with the Discovery Board is quite simple:

Move

the

soldered links on SB3 and SB7

to

SB2 an SB6.

The

n all

the

debugger signals are available on

the

headers CN2 and CN3

 

CN3  1,2,3,4 = VCC, SWCLK, GND, SWO and CN2 5,6 = RESET and SWO. 

This is a quite a good low cost development system 

#code_red #stm32-discovery #stm32f4
This topic has been closed for replies.

12 replies

frankmeyer9
Associate III
March 27, 2013
Posted on March 27, 2013 at 17:29

A personal (private) licence for Crossworks is about 1/10 of the above mentioned cost, so $150 approximately. I have one, and still view it as a good investment.

And the last time I checked CodeRed, they had limited licences for 256/512k codesize, at a price of $256 and $512 - what a coincidence ;)

But as discussed, you need to check for the debug adapter support.

CW supports both ST-Llink V1 and V2, but the former one not under Linux.

bl_it
bl_itAuthor
Associate III
March 28, 2013
Posted on March 28, 2013 at 09:13

...Yup looks like  cross works is a better option if you are not doing commercial dev, however for commercial dev they are more expensive. (also I like to support open source if I can)