Skip to main content
Associate II
Nov 29, 2024 8:03 AM UTC
Solved

Code error when passing parameters to timer function

https://community.st.com/t5/stm32-mcus-products/can-pwm-settings-affect-other-timer-settings/m-p/748254#M267471

void TIM2_Configuration(u32 Intervalms)
{
	RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

	TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

	TIM_TimeBaseStructure.TIM_Prescaler = 16000-1;

	//do not work
	//TIM_TimeBaseStructure.TIM_Period 	 = Intervalms - 1;

	//do work
	TIM_TimeBaseStructure.TIM_Period 	 = 500 - 1;
	TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
	TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

	TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
	TIM_Cmd(TIM2, ENABLE);

	NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
	NVIC_InitTypeDef NVIC_InitStructure;

	NVIC_InitStructure.NVIC_IRQChannel 					 = TIM2_IRQn;
	NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
	NVIC_InitStructure.NVIC_IRQChannelSubPriority 		 = 1;
	NVIC_InitStructure.NVIC_IRQChannelCmd 				 = ENABLE;

	NVIC_Init(&NVIC_InitStructure);
}

 In the last article, I said that the code worked or did not work depending on the location of TIM2_Configuration. However, when I removed the parameter from TIM2_Configuration and changed the period initialization to 500-1, the code worked properly regardless of the order. Does anyone know what causes this phenomenon to occur?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 29, 2024 10:39 AM UTC

Check the value of 

TIM_TimeBaseStructure.TIM_Period 

after setting it:

TIM_TimeBaseStructure.TIM_Period 	 = Intervalms - 1;

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 29, 2024 10:39 AM UTC

Check the value of 

TIM_TimeBaseStructure.TIM_Period 

after setting it:

TIM_TimeBaseStructure.TIM_Period 	 = Intervalms - 1;

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.