Skip to main content
Kevin Genskowsky
Associate
Jul 13, 2017 2:48 PM UTC
Solved

CMWX1ZZABZ Power issues Murata LRWAN1 (ver1.1.1)

Posted on July 13, 2017 at 16:48

Have been working with this guys a couple of weeks and the yare asom, but the code seems to be draining power like crasy even in stop mode 1mA.

Has any one been able to lower power consumption on stop to uA? 

    This topic has been closed for replies.
    Kevin Genskowsky
    Kevin GenskowskyBest answer
    Associate
    Jul 20, 2017 5:05 PM UTC
    Posted on July 20, 2017 at 17:05

    Yes Indead

    st.mcu

    ‌

    I disabled all led configurations and initializations. And fisicaly Conected VDD_TCX0 to PA

    and changed in mlm32l0xx_hw_conf.h

    #define RADIO_TCXO_VCC_PORT GPIOA

    #define RADIO_TCXO_VCC_PIN GPIO_PIN_10

    Seems that some more configuration could be missing in PA Will have to check more details when I have some time.

    3 replies

    Tesla DeLorean
    Guru
    Jul 13, 2017 3:07 PM UTC
    Posted on July 13, 2017 at 17:07

    Not sat and measured. Not using in Low Power/Energy mode, but code there seems poorly executed,

     bunch of grinding delay/spin loops.

    This on the DISCO or your own implementation?

    The DISCO has the TCXO strapped on all the time. You'd need to check the code build, that LOW_POWER_DISABLE is not defined.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Amel NASRI
    ST Technical Moderator
    Jul 17, 2017 2:06 PM UTC
    Posted on July 17, 2017 at 16:06

    Hi

    Genskowsky.Kevin

    ‌,

    Based on your posts in

    https://community.st.com/0D50X00009XkYNDSA3

    , your problem seems to be fixed.

    Do you confirm? Could you please update this thread with the solution you found?

    Thanks.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Kevin Genskowsky
    Kevin GenskowskyAuthorBest answer
    Associate
    Jul 20, 2017 5:05 PM UTC
    Posted on July 20, 2017 at 17:05

    Yes Indead

    st.mcu

    ‌

    I disabled all led configurations and initializations. And fisicaly Conected VDD_TCX0 to PA

    and changed in mlm32l0xx_hw_conf.h

    #define RADIO_TCXO_VCC_PORT GPIOA

    #define RADIO_TCXO_VCC_PIN GPIO_PIN_10

    Seems that some more configuration could be missing in PA Will have to check more details when I have some time.