Skip to main content
GreenGuy
Senior III
May 1, 2018
Question

CMSIS_OS.h warning - osThreadDef, warning: initialization from incompatible pointer type [-Wincompatible-pointer-types]

  • May 1, 2018
  • 1 reply
  • 1469 views
Posted on May 01, 2018 at 03:41

Has anyone seen this warning while using FreeRTOS?  The full define is :

#define osThreadDef(name, thread, priority, instances, stacksz)  \

const osThreadDef_t os_thread_def_##name = \

{ #name, (thread), (priority), (instances), (stacksz)}

This define is being used because the current FreeRTOSConfig.h has configSUPPORT_STATIC_ALLOCATION == 0.  This was taken from the tcpip RTOS example from H7_V1.2.0.

Has anyone seen this?

    This topic has been closed for replies.

    1 reply

    Stm32User
    Associate III
    September 7, 2018

    I have seen this problem when using static timers, specifically with the ​osTimerStaticDef macro, but my experiences may be of help to you or others.

    static osTimerId              IdleTimerId ;                                                                                                                     // This is the timer handle

    osStaticTimerDef_t        IdleTimerControlBlock;                                                                                                 // This is some ram for the timer

    osTimerStaticDef(IdleTimer, IdleTimer_TimeOut, &IdleTimerControlBlock);                                           // This macro creates a timer object

    Here is the macro itself:-

    #define osTimerStaticDef(name, function, control) \

    const osTimerDef_t os_timer_def_##name = \

    { (function), (control) }

    #endif

    And this is what it creates the following :-

    const osTimerDef_t os_timer_def_IdleTimer = { IdleTimer_TimeOut, &IdleTimerControlBlock };

    IdleTimer_TimeOut is a callback function pointer, &IdleTimerControlBlock is a pointer to the TCB

    I had the callback function declared as follows:-

    void IdleTimer_TimeOut(void)

    and got the warnings you mentioned. So I inspected the definition of osTimerDef_t

    typedef struct os_timer_def {

     os_ptimer                        ptimer;                  ///< start address of a timer function

     osStaticTimerDef_t       *controlblock;     ///< control block to hold timer's data for static allocation; NULL for dynamic allocation

    } osTimerDef_t;

    and then os_ptimer

    typedef void (*os_ptimer) (void const *argument);

    You can see that the call back pointer needs to correspond with this type. I changed the call back declaration as follows and the warnings went away.

    void IdleTimer_TimeOut(void const *argument)

    Hope this helps.