Skip to main content
PTuan.1
Visitor II
Aug 21, 2022 10:12 AM UTC
Question

Cmake issue: Too many levels of symbolic links

Hi all!

Currently, I create one project STM32F103 MCU with RTOS by Cmake and I got the issue when I compile the project. That is "Too many levels of symbolic links".

My cmake version is 3.22.1.

I would like to send you my CMakelists.txt file. Please check the attachment and help me figure the issue out.

Thanks and regards

# Template CMakeLists.txt configuration for STM32 MCUS
cmake_minimum_required(VERSION 3.12)
# ##############################################################################
# Edit your MCU information up to the next border
project(nrf24l01)
set(PROJECT_DIR output)
 
include(${CMAKE_CURRENT_SOURCE_DIR}/gcc-arm-none-eabi.cmake)
include(${CMAKE_CURRENT_SOURCE_DIR}/source.cmake)
 
set(PROJECT_OUTPUT_PATH /build_outputs)
if(DEFINED PROJECT_OUTPUT_PATH)
 set(BUILD_OUTPUT_DIR ${PROJECT_OUTPUT_PATH})
else()
 set(BUILD_OUTPUT_DIR ${CMAKE_CURRENT_SOURCE_DIR}/../${PROJECT_TYPE}/build_outputs)
endif()
 
set(MCU_FAMILY STM32F1xx)
set(MCU_MODEL STM32F103x6)
set(CPU_PARAMETERS
 -mcpu=cortex-m3
 )
# Some default GCC settings
set(FLAGS
 "-fdata-sections -ffunction-sections \
 --specs=nano.specs -Wl,--gc-sections")
set(CPP_FLAGS
 "-fno-rtti -fno-exceptions \
 -fno-threadsafe-statics")
 
 
set(CMAKE_TRY_COMPILE_TARGET_TYPE STATIC_LIBRARY)
 
set(STARTUP_SCRIPT ${CMAKE_CURRENT_SOURCE_DIR}/startup_stm32f103x6.s)
set(MCU_LINKER_SCRIPT ${CMAKE_CURRENT_SOURCE_DIR}/STM32F103R6Hx_FLASH.ld)
# ##############################################################################
set(EXECUTABLE ${CMAKE_PROJECT_NAME})
# enable_language(C CXX ASM)
set(CMAKE_C_STANDARD 11)
set(CMAKE_C_STANDARD_REQUIRED ON)
set(CMAKE_C_EXTENSIONS ON)
set(CMAKE_CXX_STANDARD 20)
set(CMAKE_CXX_STANDARD_REQUIRED ON)
set(CMAKE_CXX_EXTENSIONS ON)
 
# Executable files
add_executable(${EXECUTABLE}
 ${STM32CUBEMX_SOURCES}
 ${PROJECT_SOURCES}
 ${STARTUP_SCRIPT})
 
# Embedded macros(defines)
target_compile_definitions(${EXECUTABLE} PRIVATE
 ${MCU_MODEL}
 USE_HAL_DRIVER)
 
# Add header directories (AFTER add_executable !!)
target_include_directories(${EXECUTABLE} PRIVATE
 ${CUBEMX_INCLUDE_DIRECTORIES}
 ${PROJECT_INCLUDE_DIRECTORIES})
 
# Compiler and linker options
target_compile_options(${EXECUTABLE} PRIVATE
 ${CPU_PARAMETERS}
 -Wall
 -Wextra
 -Wpedantic
 -Wno-unused-parameter
 $<$<COMPILE_LANGUAGE:CXX>:
 -Wno-volatile
 -Wold-style-cast
 -Wuseless-cast
 -Wsuggest-override>
 $<$<CONFIG:Debug>:-Og -g3 -ggdb>
 $<$<CONFIG:Release>:-Og -g0>)
 
target_link_options(${EXECUTABLE} PRIVATE
 -T${MCU_LINKER_SCRIPT}
 ${CPU_PARAMETERS}
 -Wl,-Map=${CMAKE_PROJECT_NAME}.map
 --specs=nosys.specs
 -Wl,--start-group
 -lc
 -lm
 -lstdc++
 -Wl,--end-group
 -Wl,--print-memory-usage)
 
add_custom_command(TARGET ${EXECUTABLE} POST_BUILD
 COMMAND ${CMAKE_SIZE} $<TARGET_FILE:${EXECUTABLE}>)
 
add_custom_command(TARGET ${EXECUTABLE} POST_BUILD
 COMMAND ${CMAKE_OBJCOPY} -O ihex $<TARGET_FILE:${EXECUTABLE}>
 ${EXECUTABLE}.hex
 COMMAND ${CMAKE_OBJCOPY} -O binary $<TARGET_FILE:${EXECUTABLE}>
 ${EXECUTABLE}.bin)

This topic has been closed for replies.