Skip to main content
paul0208
Associate III
February 6, 2016
Question

Clock setting for stm32f105rc

  • February 6, 2016
  • 2 replies
  • 753 views
Posted on February 06, 2016 at 16:12

I made a custom board using stm32f105rc with external 8MHz x-tal.

I think I would set the system clock with HSE,PLL,72MHz.

But each stm32f105 board's SysTick_Handler timing are not same. 10,000 tick is 1 sec. 

In some board, 9645 tick is 1 sec, for other board, 9834 tick is 1 sec.... 

I think the system is not set to HSE/PLL, but HSI. But I'm not sure. Just guessing from different SysTick for all the board.

My program regarding clock setting are bellow.

----------

stmf1xx.h

#if !defined (STM32F10X_LD) && !defined (STM32F10X_LD_VL) && !defined (STM32F10X_MD) && !defined (STM32F10X_MD_VL) && !defined (STM32F10X_HD) && !defined (STM32F10X_HD_VL) && !defined (STM32F10X_XL) && !defined (STM32F10X_CL) 

  /* #define STM32F10X_LD */     /*!< STM32F10X_LD: STM32 Low density devices */

  /* #define STM32F10X_LD_VL */  /*!< STM32F10X_LD_VL: STM32 Low density Value Line devices */  

//#define STM32F10X_MD    /*!< STM32F10X_MD: STM32 Medium density devices */

  /* #define STM32F10X_MD_VL */  /*!< STM32F10X_MD_VL: STM32 Medium density Value Line devices */  

#define STM32F10X_HD     /*!< STM32F10X_HD: STM32 High density devices */

//#define STM32F10X_HD_VL  /*!< STM32F10X_HD_VL: STM32 High density value line devices */  

  /* #define STM32F10X_XL */     /*!< STM32F10X_XL: STM32 XL-density devices */

//#define STM32F10X_CL     /*!< STM32F10X_CL: STM32 Connectivity line devices */

#endif

system_stm32f1xx.c

#if defined (STM32F10X_LD_VL) || (defined STM32F10X_MD_VL) || (defined STM32F10X_HD_VL)

// #define SYSCLK_FREQ_HSE    HSE_VALUE

// #define SYSCLK_FREQ_24MHz  24000000

#else

// #define SYSCLK_FREQ_HSE    HSE_VALUE

/* #define SYSCLK_FREQ_24MHz  24000000 */ 

//#define SYSCLK_FREQ_36MHz  36000000

/* #define SYSCLK_FREQ_48MHz  48000000 */

/* #define SYSCLK_FREQ_56MHz  56000000 */

#define SYSCLK_FREQ_72MHz  72000000

#endif

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    February 6, 2016
    Posted on February 06, 2016 at 18:04

    Aren't these Connectivity Line (CL) parts?

    http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1031/LN1564/PF221023

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    paul0208
    paul0208Author
    Associate III
    February 8, 2016
    Posted on February 08, 2016 at 04:30

    Thank you. clive1.

    I wonder why I thought 105RC was HD device...

    You changed your avatar.^^