Skip to main content
eleventen
Associate III
February 16, 2012
Question

Clock for ULPI PHY?

  • February 16, 2012
  • 3 replies
  • 1069 views
Posted on February 16, 2012 at 22:17

Greetings,

We're having a hard time telling whether or not the STM32F207 will drive the clock for the PHY.  There is a sentence in the datasheet that says, vaguely

   External HS or HS OTG operation supporting ULPI in SDR mode. The OTG PHY is

connected to the microcontroller ULPI port through 12 signals. It can be clocked using

the 60 MHz output.

Does this mean we have to use one of the MCO outputs?  Or will the ULPI clock be driven at 60MHz?
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 16, 2012
    Posted on February 16, 2012 at 22:31

    We're having a hard time telling whether or not the STM32F207 will drive the clock for the PHY.  There is a sentence in the datasheet that says, vaguely

     

     

    External HS or HS OTG operation supporting ULPI in SDR mode. The OTG PHY is connected to the microcontroller ULPI port through 12 signals. It can be clocked using the 60 MHz output.

     

     

    Does this mean we have to use one of the MCO outputs?  Or will the ULPI clock be driven at 60MHz?

    Or PA.5 OTG_HS_ULPI_CK

    12-pin interface

    CLK    PA5

    DIR    PI11

    STP    PC0

    NXT    PH4

    D0    PA3

    D1    PB0

    D2    PB1

    D3    PB10

    D4    PB11

    D5    PB12

    D6    PB13

    D7    PB5

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    eleventen
    eleventenAuthor
    Associate III
    February 16, 2012
    Posted on February 16, 2012 at 23:27

    We're having a hard time telling whether or not the STM32F207 will drive the clock for the PHY.  There is a sentence in the datasheet that says, vaguely

     

     

    External HS or HS OTG operation supporting ULPI in SDR mode. The OTG PHY is connected to the microcontroller ULPI port through 12 signals. It can be clocked using the 60 MHz output.

     

     

    Does this mean we have to use one of the MCO outputs?  Or will the ULPI clock be driven at 60MHz?

    Or PA.5 OTG_HS_ULPI_CK

    According to the UPLI spec, this line can be driven by the MCU or the PHY.  We just want to know that the MCU *does* drive it.  The RCC clock tree doesn't give me any place to configure a PLL or divider to get the 60MHz clock.

    Tesla DeLorean
    Guru
    February 16, 2012
    Posted on February 16, 2012 at 23:54

    ''The USB OTG HS (60 MHz) clock which is provided from the external PHY''

    The STUPLI01B outputs 60 MHz, generated via it's external 26MHz crystal

    http://www.st.com/internet/analog/product/189049.jsp

    Presuming your part is running at 120 MHz,

    MCO1 = PLL / 2,  60 MHz

    MCO2 = PLL / 2,  60 MHz

    MCO2 = SYSCLK / 2, 60 MHz

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..