Skip to main content
Dilbert K
Associate III
Nov 23, 2017 12:16 AM UTC
Question

Client mode for X-NUCLEO-IDB05A1

Posted on November 23, 2017 at 01:16

I just started with the 

X-NUCLEO-IDB05A1 board which has the 

SPBTLE-RF BlueNRG-MS RF module.

I would like to focus on the 'Client mode' for this project.  Have downloaded the 'STM32CubeExpansion_BLE1_V3.2.0\Projects\Multi\Applications\SampleAppThT' and able to load and run the project in Client mode.

However, I need to get deeper, is there more example project ST has available for Client specific ?

like getting BLE device list and getting Advertise data of connected device...

What document would be best for BLE Client Stack study ?

Thanks so much.

    This topic has been closed for replies.

    10 replies

    Antonio Vilei
    ST Employee
    Nov 23, 2017 10:59 AM UTC
    Posted on November 23, 2017 at 11:59

    Hi Dilbert K,

    if you need more information about the Central role, like scanning, connecting to peripherals,performing services and characteristics discovery, I suggest to use the

    /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fst_com%2Fen%2Fproducts%2Fembedded-software%2Fwireless-connectivity-software%2Fstsw-bnrgui.html

    tool.

    In the 'ACI Utilities' tab, ithas someinteractive features related to the Central Role that will let you get deeper. After you use those features,you can review the individual commands and events being generated.

    In order to use the GUI, please make sure that your STM32 board isrunning the Virtual_COM_Port project of the X-CUBE-BLE1 package.

    The BlueNRG GUI alsoincludes a set of scripts that you can run by usingits built-in interpreter. Starting from the rootof the tool installation folder, you can find them in the 'Application\scripts'. You'll find examples for many use cases, involving multiple connections, security, whitelist and so on.

    These scripts are written in Python, but you can easilyget inspiration from them for your own C code.

    Best regards,

    Antonio

    Dilbert K
    Dilbert KAuthor
    Associate III
    Nov 23, 2017 4:02 PM UTC
    Posted on November 23, 2017 at 17:02

    Thanks for the info...however, I am trying to do a BLE hub using 

    SPBTLE-RF, this is why I want some sample from ST in term of API of the stack.

    I had been using the SensorTile platform for some time but all the code is on Server side.

    Antonio Vilei
    ST Employee
    Nov 23, 2017 5:56 PM UTC
    Posted on November 23, 2017 at 17:56

    Hi Dilbert K,

    what do you exactly mean by BLE hub?

    The SampleAppThT application that you have already used shows how to implement a GATT Client with SPBTLE-RF configured as Central.

    The

    http://www.st.com/content/ccc/resource/technical/document/programming_manual/1c/7e/d3/a6/d0/52/4a/35/DM00141271.pdf/files/DM00141271.pdf/jcr:content/translations/en.DM00141271.pdf

     programming manual 'BlueNRG, BlueNRG-MS stacks programming guidelines' provides details about how to program BlueNRG-MS (the chip that is used in your SPBTLE-RF module), including information about the client side.

    If you want a more advanced example about how to use a single SPBTLE-RF client that can connect to multiple servers and get information from them, please refer to the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-net-blestar1.html

    software package.

    This package shows how to create a star-topology network of BLE devices. Before trying this example, however, I recommend going through the BlueNRG GUI as I suggested in my previous post, as this will help you learn the basics, first. The BlueNRG GUI works fine with SPBTLE-RF.

    Best regards,

    Antonio

    Dilbert K
    Dilbert KAuthor
    Associate III
    Nov 23, 2017 11:38 PM UTC
    Posted on November 23, 2017 at 23:38

    Yes, I am.  BLE hub connecting to multiple BLE devices and send data out to WiFi.

    The FP-NET_BLESTART1 is what I want.

    I had scan through the PM0237 and locate the section for setup multiple connections...but doc is out dated compare to recent release code.

    I tried following the doc and add following to set the stack mode

    uint8_t stackmode[1]={0x03}; // mode 3 or 4

    ret = aci_hal_write_config_data(CONFIG_DATA_MODE_OFFSET, CONFIG_DATA_MODE_LEN, stackmode);

    ret = aci_gap_init_IDB05A1(GAP_CENTRAL_ROLE_IDB05A1 | GAP_PERIPHERAL_ROLE_IDB05A1, 0, 0x07, &service_handle, &dev_name_char_handle, &appearance_char_handle);

    But the 2nd connection of following call still come back with Error = 0x41.

      ret = aci_gap_create_connection(0x0010,0x0010, PUBLIC_ADDR, bdaddr, PUBLIC_ADDR, 0x6c, 0x6c, 0,

    0xc80, 0x000c ,0x000c);

     

    I will go over the 

    BLESTART1 and see I could find the code accordingly.

    Antonio Vilei
    ST Employee
    Nov 24, 2017 10:53 AM UTC
    Posted on November 24, 2017 at 11:53

    What is the current firmware version of your BlueNRG-MS devices?

    Please make sure that you are using the latest version (7.2c as of now) of the BlueNRG-MS firmware on all of your SPBTLE-RF modules.

    The tool and the readme with instructions for updating the BlueNRG-MS firmware can be found in

    the Utilities/PC_Software/FlashUpdaterTool folder of the X-CUBE-BLE1 package.

    Best regards,

    Antonio

    Dilbert K
    Dilbert KAuthor
    Associate III
    Nov 24, 2017 10:29 PM UTC
    Posted on November 24, 2017 at 22:29

    I had just updated

    SPBTLE-RF(

    BlueNRG-MS) to V7.2c yesterday using the tools.

    But result the same.. got error on 2nd connection...

    I search through the '

    FP-NET_BLESTART1

    ' it is using the same code for both 

    aci_hal_write_config_data & 

    aci_gap_init_IDB05A1

    Is there extra API need to call after 1st device connected ? before calling 

    aci_gap_create_connection 2nd time ?