Skip to main content
casainho
Associate
February 14, 2013
Question

Clearing the OCxREF signal on an external event

  • February 14, 2013
  • 6 replies
  • 1584 views
Posted on February 14, 2013 at 14:30

Hello.

As described on STM32F100 manual:

The OCxREF signal for a given channel can be driven Low by applying a High level to the ETRF input (OCxCE enable bit of the corresponding TIMx_CCMRx register set to ‘1’). The OCxREF signal remains Low until the next update event, UEV, occurs.

 

 

For example, the OCxREF signal) can be connected to the output of a comparator to be used for current handling.

 

I am trying to do this, and I am using 3 PWM for BLDC motor control (wich works very well for now but lacks current control). I am using OC1, OC2 and OC3 for PWM generation.

When ETR pin is active (output of a LM258 comparator when over current), ONLY the OC3Ref signal is clear and so I only get PWM channel 3 off on over current while channel 1 and 2 should also be off.

Where is the code configuration for ETR:

GPIO_InitStructure

.

GPIO_Pin

=

GPIO_Pin_12

;

GPIO_InitStructure

.

GPIO_Mode

=

GPIO_Mode_IN_FLOATING

;

GPIO_InitStructure

.

GPIO_Speed

=

GPIO_Speed_50MHz

;

GPIO_Init

(

GPIOA

,

&

GPIO_InitStructure

);

  

/* configure ETR for current control */

  

TIM_ETRConfig

(

TIM1

,

TIM_ExtTRGPSC_OFF

,

TIM_ExtTRGPolarity_NonInverted

,

0

);

  

TIM_ClearOC1Ref

(

TIM1

,

TIM_OCClear_Enable

);

  

TIM_ClearOC2Ref

(

TIM1

,

TIM_OCClear_Enable

);

  

TIM_ClearOC3Ref

(

TIM1

,

TIM_OCClear_Enable

);

My code is here:

https://github.com/casainho/EBike-Smart-Controller/blob/8461b455ac4f96b2241e3a312c9c726ff0795221/firmware/pwm.c

This is an OpenSource motor BLDC controller, project page: 

http://smartebike.likesyou.org/

Right now the motor works very well, including the Hall Sensor and Brake (using STM32 hardware for this). The only thing missing is over current control.

Thank you in advance.
    This topic has been closed for replies.

    6 replies

    waclawek.jan
    Super User
    February 15, 2013
    Posted on February 15, 2013 at 11:45

    Check (read out in real application) content of TIM1_CCMR1 and TIM1_CCMR2.

    JW
    casainho
    casainhoAuthor
    Associate
    February 16, 2013
    Posted on February 16, 2013 at 14:00

    Thank you. Now the code works perfect.

    I were doing this during the program to turn off the PWM:

    TIM_ForcedOC2Config(TIM1, TIM_ForcedAction_InActive); // disable PWM

    Turns out that it changed the initial configuration.

    casainho
    casainhoAuthor
    Associate
    February 19, 2013
    Posted on February 19, 2013 at 23:03

    I recorded a video showing current control working:

    http://www.youtube.com/watch?v=i0VohXLZfCA

    Nickname12657_O
    Associate III
    February 19, 2013
    Posted on February 19, 2013 at 23:20

    0690X0000060MlyQAE.gif

    waclawek.jan
    Super User
    February 20, 2013
    Posted on February 20, 2013 at 11:27

    I don't get it - TIM_ForcedOC2Config() is not supposed to change the OC2CE bit, so it should not affect the PWM behaviour once it's restored.

    Or have I overlooked something?

    JW

    casainho
    casainhoAuthor
    Associate
    February 22, 2013
    Posted on February 22, 2013 at 23:42

    Seems that TIM_ForcedOC2Config() disables PWM1 mode I am using and so when configuring again to PWM1 mode is needed to setup the correct bits again. Maybe leaving out PWM1 mode ''resets'' some bits on the register.