Skip to main content
cyrildufoing
Associate
Dec 20, 2015 7:58 PM UTC
Question

Circular buffer

Posted on December 20, 2015 at 20:58

Someone knows how to implement a circular buffer with HAL Drivers F1? 

    This topic has been closed for replies.

    5 replies

    carmine
    Associate III
    Dec 20, 2015 9:54 PM UTC
    Posted on December 20, 2015 at 22:54

    You can find several good implementations around on the web. Google knows about them.

    There are no special requirements for using a ring buffer on a STM32 MCU. For example, you can consider

    https://github.com/cnoviello/mastering-stm32/tree/master/nucleo-f103RB/Middlewares/RingBuffer

     even if I don't like it too much (it could be implemented in a faster way if it's ok to lose a bit of ''safeness''). Please, consider that this library works well only if you have just two ''threads'' operating on it. Otherwise, you have to add locking mechanisms. 

    Senior
    Mar 6, 2024 6:25 PM UTC

    Hi Carmine,

    Thanks for your post.

    One question for you and I would be very glad if you could answer. I am using STM32F407VG-DISC1 board.

    I have checked the repo you ve provided. I wonder that, is that OK if I copy ringbuffer.c under core-->src and also ringbuffer.h under core -->inc.

    Then, can I use ringbuffer functions with ease ?

    demir_0-1709749501221.png

     

    Tesla DeLorean
    Guru
    Mar 6, 2024 7:31 PM UTC

    You're responding to a very old post, I think several forum transitions ago, the OP might not respond.

    I'd imagine you can use C rule to determine how best to integrate this into your build. Ring / Circular buffers being a pretty basic concept.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tm3341
    Associate III
    Dec 21, 2015 11:44 AM UTC
    Posted on December 21, 2015 at 12:44

    Check this ''thread'' safe implementation.

    https://github.com/MaJerle/stm32fxxx_hal_libraries/blob/master/00-STM32_LIBRARIES/tm_stm32_buffer.h

    If you don't use my libs, then just remove includes for libraries in this library:

    //Remove these 2 lines:

    #include ''stm32fxxx_hal.h''

    #include ''defines.h''

    And you are ready to go.

    Lib supports memory allocation with malloc, or if you want, you specify it by yourself.

    Ask here for more info, if needed.