Skip to main content
KN.2
Associate II
March 20, 2020
Question

circuit working when connect jtag ground or cro ground

  • March 20, 2020
  • 0 replies
  • 446 views

hi,

we are developing HMI using stm32f746 microcontroller it has 7 inch tft display,sd ram,norflash,usb,sdcard,ethernet and wifi.and we are devoloping a code for each sections one by one,till now tft display ethernet uart,wifi sections are completed,when test the wifi code if i press reset the microcontroller is noy getting on(cpu run led is not blinking,no display )if i connect the j tag ground alone with this its working similarly when i connect the negative probe of cro with any ground terminal its working but its not a fixed issue this is happening in random manner.any idea???

This topic has been closed for replies.