Question
Choosing GPIO Speed Setting
Posted on June 19, 2015 at 13:27
Hello,
what is a sensible relation between the GPIO speed setting and peripheral device speed? E.g. OSPEED = 00 on a >2.7 Volt STM32F42x with 10 pF load has a value of 8 MHz max. Is that good for a SPI clock rate of 8 MHz? Or should OSPEED be substantial higher than the peripheral clock speed? What strategy to use?