Skip to main content
MKim.12
Associate
February 7, 2023
Question

charger detect problem

  • February 7, 2023
  • 0 replies
  • 934 views

Hello,

I’m using STM32L412RB.

I'm trying to differentiate between the types of chargers

When the charger is connected, reboot occurs, and I run HAL_PCDEx_ActivateBCD()/HAL_PCDEx_BCD_VBUSDetect() in MX_USB_DEVICE_Init().

After that, in case of abnormality, HAL_PCDEx_ActivateBCD()/HAL_PCDEx_BCD_VBUSDetect() is used to detect charger at regular intervals.

In the example(\STM32Cube_FW_L4_V1.16.0\Projects\NUCLEO-L412RB-P\Applications\USB_Device\HID_Standalone_BCD) an interrupt occurs when Vbus detect is performed, and HAL_PCDEx_BCD_VBUSDetect() is performed within it.

My board does not detect Vbus, but performs HAL_PCDEx_ActivateBCD()/HAL_PCDEx_BCD_VBUSDetect().

I tried using the callback function within HAL_PCDEx_BCD_VBUSDetect() and also tried saving the value directly within the function.

The data identified at this time are randomly different.

1. In case of 1 byte save

 - Check PCD_BCD_ERROR

2. In case of 2 byte save

 - Check PCD_BCD_CONTACT_DETECTION

 - Check PCD_BCD_DISCOVERY_COMPLETED

3. In case of 3 byte save

 - Check PCD_BCD_CONTACT_DETECTION

 - Check PCD_BCD_STD_DOWNSTREAM_PORT or PCD_BCD_CHARGING_DOWNSTREAM_PORT

 - Check PCD_BCD_DISCOVERY_COMPLETED

In the above three cases, the third one seems to be normal, but the actual SDP/CDP cannot be distinguished.

In terms of HW, the DP/DM ports are connected to the MCU through the USB switch, and each TVS is installed before the USB switch.

If this method is wrong, what should I check?

 thank you

 

 

 

void MX_USB_DEVICE_Init(void)

{

 /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

 /* USER CODE END USB_DEVICE_Init_PreTreatment */

 /* Init Device Library, add supported class and start the library. */

 if (USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_Start(&hUsbDeviceFS) != USBD_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

 // charger detect enable

 HAL_PCDEx_ActivateBCD(&pcd);

 HAL_PCDEx_BCD_VBUSDetect(&pcd);

 /* USER CODE END USB_DEVICE_Init_PostTreatment */

}

void HAL_PCDEx_BCD_VBUSDetect(PCD_HandleTypeDef *hpcd)

{

 USB_TypeDef *USBx = hpcd->Instance;

 uint32_t tickstart = HAL_GetTick();

 /* Wait Detect flag or a timeout is happen*/

 while ((USBx->BCDR & USB_BCDR_DCDET) == 0U)

 {

  /* Check for the Timeout */

  if ((HAL_GetTick() - tickstart) > 1000U)

  {

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

   hpcd->BCDCallback(hpcd, PCD_BCD_ERROR);

#else

  #if defined(BCD_Callback_USE)

   HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_ERROR);

  #else

   charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_ERROR;

   charger_state.pcdInfoOrder++;

  #endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

   return;

  }

 }

 HAL_Delay(200U);

 /* Data Pin Contact ? Check Detect flag */

 if ((USBx->BCDR & USB_BCDR_DCDET) == USB_BCDR_DCDET)

 {

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

  hpcd->BCDCallback(hpcd, PCD_BCD_CONTACT_DETECTION);

#else

 #if defined(BCD_Callback_USE)

  HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CONTACT_DETECTION);

 #else

  charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_CONTACT_DETECTION;

  charger_state.pcdInfoOrder++;

 #endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

 }

 /*Primary detection: checks if connected to Standard Downstream Port

 (without charging capability) */

 USBx->BCDR &= ~(USB_BCDR_DCDEN);

 HAL_Delay(50U);

 USBx->BCDR |= (USB_BCDR_PDEN);

 HAL_Delay(50U);

 /* If Charger detect ? */

 if ((USBx->BCDR & USB_BCDR_PDET) == USB_BCDR_PDET)

 {

  /* Start secondary detection to check connection to Charging Downstream

  Port or Dedicated Charging Port */

  USBx->BCDR &= ~(USB_BCDR_PDEN);

  HAL_Delay(50U);

  USBx->BCDR |= (USB_BCDR_SDEN);

  HAL_Delay(50U);

  /* If CDP ? */

  if ((USBx->BCDR & USB_BCDR_SDET) == USB_BCDR_SDET)

  {

   /* Dedicated Downstream Port DCP */

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

   hpcd->BCDCallback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);

#else

  #if defined(BCD_Callback_USE)

   HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DEDICATED_CHARGING_PORT);

  #else

   charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_DEDICATED_CHARGING_PORT;

   charger_state.pcdInfoOrder++;

  #endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

  }

  else

  {

   /* Charging Downstream Port CDP */

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

   hpcd->BCDCallback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);

#else

  #if defined(BCD_Callback_USE)

   HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_CHARGING_DOWNSTREAM_PORT);

  #else

   charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_CHARGING_DOWNSTREAM_PORT;

   charger_state.pcdInfoOrder++;

  #endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

  }

 }

 else /* NO */

 {

  /* Standard Downstream Port */

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

  hpcd->BCDCallback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);

#else

 #if defined(BCD_Callback_USE)

  HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_STD_DOWNSTREAM_PORT);

 #else

  charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_STD_DOWNSTREAM_PORT;

  charger_state.pcdInfoOrder++;

 #endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

 }

 /* Battery Charging capability discovery finished Start Enumeration */

 (void)HAL_PCDEx_DeActivateBCD(hpcd);

#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)

 hpcd->BCDCallback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);

#else

#if defined(BCD_Callback_USE)

 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);

#else

 charger_state.pcdInfo[charger_state.pcdInfoOrder] = PCD_BCD_DISCOVERY_COMPLETED;

 charger_state.pcdInfoOrder++;

#endif

#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

}

This topic has been closed for replies.