Skip to main content
pdowns
Associate
February 19, 2009
Question

Change USART baud rate on the fly?

  • February 19, 2009
  • 3 replies
  • 825 views
Posted on February 19, 2009 at 10:58

Change USART baud rate on the fly?

    This topic has been closed for replies.

    3 replies

    m3allem
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:03

    Hi pdowns;

    In your code, you have only disable the receive interrupt, and the transmit interrupt was not disabled:

    /* DISABLE USART2 Receive and Transmit interrupts */

    USART_ITConfig(USART2, USART_IT_RXNE, DISABLE);

    May this has caused your problem!!

    B.R.

    M3allem

    [ This message was edited by: M3allem on 19-02-2009 10:15 ]

    [ This message was edited by: M3allem on 19-02-2009 10:16 ]

    pdowns
    pdownsAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:03

    Can someone tell me the procedure to change the baud rate on the USART once it has already been initialized? I have a module that I communicate with using USART2 and I need to be able to change the baud rate on the module then change the USART baud rate on the STM32. I am using a the rxne interrupt to receieve data. This is my code to try and change the baud rate.

    void UART_ChangeBaud(u32 UartSpeed)

    {

    USART_InitTypeDef USART_InitStructure;

    GPIO_InitTypeDef GPIO_InitStructure;

    /* DISABLE USART2 Receive and Transmit interrupts */

    USART_ITConfig(USART2, USART_IT_RXNE, DISABLE);

    USART_InitStructure.USART_BaudRate = UartSpeed;//9600;//115200;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No ;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS;

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    USART_Init(USART2, &USART_InitStructure);

    USART_ClearFlag(USART2, USART_FLAG_RXNE);

    USART_ClearITPendingBit(USART2, USART_IT_RXNE);

    /* Enable USART2 Receive and Transmit interrupts */

    USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);

    //USART_ITConfig(USART2, USART_IT_TXE, ENABLE);

    /* Enable the USART2 */

    USART_Cmd(USART2, ENABLE);

    return;

    }

    Is my procedure incorrect? Once I try to change the baud rate I can't receive anything from the module.

    pdowns
    pdownsAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:03

    I don't think it is that, I only use the RX interrupt. I never enabled the TX intterrupt, I just forgot to edit the comments.